Linux device driver for OnSemi AR0230CS camera sensor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Linux device driver for OnSemi AR0230CS camera sensor

5,959件の閲覧回数
asharma
Contributor II

Hi All,

We are trying to connect camera sensor OnSemi AR0230CS (ON Semiconductor) to Boundary devices BD-SL-I.MX6 (i.MX6 ARM Development Board) on parallel interface.

The problem is that there is no Linux driver for this sensor, So I guess we have to write a new one.

It would be helpful, if you could point me from where I can start and a reference camera device driver which I can refer to write driver for AR0230CS.

Thank you in advance.

ラベル(3)
2 返答(返信)

5,198件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Abhishek

please check Boundary Devices OV5642 links and attached Linux Manual.

OV5642 auto-focus on i.MX6 - Boundary Devices 

ENGR00169489-1 Add OV5642 csi camera support for i.mx6 sabre-lite board. (379843df) · Commits · ARM ... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

5,198件の閲覧回数
asharma
Contributor II

Hi Igor,

Thanks for your reply.

Provided links and pdf are helpful.

Do you also have a programming manual for camera driver for i.MX6s, as camera drivers written for freescale look different from general camera drivers.

Thanks.

Abhishek

0 件の賞賛
返信