Linux Image/Text Display Application using Yocto

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Linux Image/Text Display Application using Yocto

1,676件の閲覧回数
barish_malshika
Contributor I
Hello everyone,
We are using the i.MX8QXP MEK development board and we are developing Linux-based applications in Yocto.
We have connected the LVDS to the HDMI converter (connected to LVDS0) to connect with the external display monitor.
We can load and boot, u-boot and Linux with rootfs from the emmc card. We can see the splash screen on the HD display in u-boot as well as Linux.
We are trying to develop a user application to display the .jpeg/.jpg HD images(1080p) and user text (logs/ text files) on the HD display.
We are using the following components:
  • Kernel version: L5.4.24_2.1.0
  • Image: core-image-base
  • Distro: x-Wayland
Please suggest a reference/way for developing an application with given components and hardware.
Thank you
1 返信

1,609件の閲覧回数
art
NXP Employee
NXP Employee

Your question seems not to be specific to any of the NXP products, but to be a kind of general Linux development question.

So, first, please refer to generally available Linux developer resources.

Some general Linux development related Application Note documents are available from NXP:

https://www.nxp.com/docs/en/application-note/AN3870.pdf https://www.nxp.com/docs/en/application-note/AN4553.pdf

Also, please refer to the documentation, specific to the Linux BSP you use.

Best Regards,

Artur

0 件の賞賛
返信