Linux Drivers for i.MX6ULL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Linux Drivers for i.MX6ULL

跳至解决方案
1,938 次查看
khollar
NXP Employee
NXP Employee

Which Linux display drivers are available, and also what LCD Digital Drivers are supported with any existing Linux drivers?

 

Ideally something similar to the Himax HX8238-D see attached, we would like to use in the 8bit data/ SPI control mode.

0 项奖励
回复
1 解答
1,726 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

The default BSP Supports SEIKO WVGA panel. For i.MX 6UltraLite, i.MX 6ULL and i.MX 7Dual SABRE-SD, it supports Embest LCD8000-43T LCD panel.The LCD interface driver supports the Samsung LMS430xx 4.3" WQVGA LCD panel.

mxc_lcdif.c Display Driver for CLAA-WVGA and SEIKO-WVGA LCD support.Here if you want to use other LCD, you can connect and porting the screen driver to your board.

All the function and BSP Supported Features you can see the documents i.MX_Linux_Release_Notes.pdf and i.MX_Linux_Reference_Manual.pdf.
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,727 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

The default BSP Supports SEIKO WVGA panel. For i.MX 6UltraLite, i.MX 6ULL and i.MX 7Dual SABRE-SD, it supports Embest LCD8000-43T LCD panel.The LCD interface driver supports the Samsung LMS430xx 4.3" WQVGA LCD panel.

mxc_lcdif.c Display Driver for CLAA-WVGA and SEIKO-WVGA LCD support.Here if you want to use other LCD, you can connect and porting the screen driver to your board.

All the function and BSP Supported Features you can see the documents i.MX_Linux_Release_Notes.pdf and i.MX_Linux_Reference_Manual.pdf.
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复