Linux Drivers for SGTL5000

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Linux Drivers for SGTL5000

ソリューションへジャンプ
7,240件の閲覧回数
anandmeharwade
Contributor II

Hi,

I am using I.MX6Q module in my design. Where could I get the Linux Drivers for SGTL5000 Audio codec

Please do share me the link for the same. For any more information feel free to reply me.

Regards

Anand Meharwade

ラベル(2)
0 件の賞賛
返信
1 解決策
5,942件の閲覧回数
gary_bisson
Senior Contributor III
4 返答(返信)
5,943件の閲覧回数
gary_bisson
Senior Contributor III
5,941件の閲覧回数
anandmeharwade
Contributor II

Dear Gary Bisson,

I have used your drivers for SGTL5000 and added into my software package. The device probing is successful and shows up the alsa device list.

When I run the 1kHz sine wave .wav file using aplay command, I am observing the signals on LINE OUT_L only and no signals at LINE OUT_R. Also the signal at LINE OUT_L is not as expected (>>>1Khz its varying frequency and doesn't look like sine wave)

Could you please let me if any other commands to be executed before running the aplay command.

For any clarification feel free to ask me. Thanks for the support

Thanks

Anand M

0 件の賞賛
返信
5,941件の閲覧回数
anandmeharwade
Contributor II

Hi Gary Bisson,

Thanks for sharing the links for the drivers. Appriciate your help and quick response.

Thanks

Anand M

5,941件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

also may be useful to look at programming guides on

Ultra-Low-Power Audio Codec|NXP 

Best regards
igor

0 件の賞賛
返信