Linux Backports into LTIB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Linux Backports into LTIB

ソリューションへジャンプ
3,225件の閲覧回数
JeromeBaron
Contributor II

HI everyone,

I am working on a board with a imx28. Right now, I use the mx28EVK. I want to include a driver for a wireless lan chipset, the TI wl18xx. I want to use the linux backports package that can be found here:

https://backports.wiki.kernel.org/index.php/Main_Page

I want to include this in my LTIB package, but I don't understand how to make it appear in the menuconfig. I know I must do a backports.spec file in my folder in dist\lfs-5.1\backports but I dont know what to put in it. I saw on the backports wiki the "build section" to put in this file, but I can find the rest of the file.

Not sure if I need to include this folder in another file to make it appear in the configuration screen of ltib.

Best regards,

Jerome

*I succesfully modified packages.lkc and pkg_map to add the package to the config screen. For now, it wont compile because of the build section.

Message was edited by: Jerome Baron

ラベル(1)
0 件の賞賛
返信
1 解決策
2,994件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jerome

I think attached appnote may help.

Best regards

igor

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,995件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jerome

I think attached appnote may help.

Best regards

igor

0 件の賞賛
返信