Linux BSP source code for i.MX7D-SABRE board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Linux BSP source code for i.MX7D-SABRE board

2,883 Views
vijayhs
Contributor I

Hi,

From where to download the Linux BSP source code for i.MX7D-SABRE board?

Thanks & Regards

Vijay H.S

Labels (1)
0 Kudos
Reply
2 Replies

2,583 Views
vijayhs
Contributor I

Hi igorpadykov,

Thank you very much for the information. I will go through the User Guide.

Thanks & Regards

Vijay H.S

0 Kudos
Reply

2,583 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vijay

yocto automatically find sources, please follow attached Yocto Guide, select configuration as described in

sect.5.1 Build configurations. BSP location is

http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/tree/?id=rel_imx_4.1.15_2.0.0_ga&h=imx_4.1.1...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply