Hello,
I am trying to port Linux version 3.10.17 to an i.MX6 SOLO (Not Solo Lite)
I started from the imx6q-sabresd configuration as foudation for the first test
make imx_v7_defconfig
make -j4 uImage LOADADDR=0x10008000
make imx6q-sabresd.dtb
Is this the correct way to proceed for MX6 SOLO ?
The problem is that kernel hangs at the line below just after trying to mount the mmcblk0
Sometimes some messages appear but they don't give much information.
I need a help to understand where to dig in order to continue the boot process.
Thank you
[BOOT LOG]
Booting Linux on physical CPU 0x0
Linux version 3.10.17+g232293e (koan@kmobile) (gcc version 4.8.2 (GCC) ) #46 SMP PREEMPT Sun Mar 1 16:04:32 CET 2015
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: Freescale i.MX6 Quad/DualLite (Device Tree)
cma: CMA: reserved 320 MiB at 3a000000
Memory policy: ECC disabled, Data cache writealloc
PERCPU: Embedded 9 pages/cpu @816f2000 s12992 r8192 d15680 u36864
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 260096
Kernel command line: console=ttymxc0,115200 maxcpus=1 root=/dev/mmcblk1p2 rootwait rw
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
Memory: 1024MB = 1024MB total
Memory: 695876k/695876k available, 352700k reserved, 0K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
vmalloc : 0xc0800000 - 0xff000000 (1000 MB)
lowmem : 0x80000000 - 0xc0000000 (1024 MB)
pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)
modules : 0x7f000000 - 0x7fe00000 ( 14 MB)
.text : 0x80008000 - 0x80d60358 (13665 kB)
.init : 0x80d61000 - 0x80de42c0 ( 525 kB)
.data : 0x80de6000 - 0x80e54670 ( 442 kB)
.bss : 0x80e54670 - 0x80edf36c ( 556 kB)
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
Preemptible hierarchical RCU implementation.
RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1.
NR_IRQS:16 nr_irqs:16 16
L310 cache controller enabled
l2x0: 16 ways, CACHE_ID 0x410000c8, AUX_CTRL 0x32050000, Cache size: 524288 B
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms
CPU identified as i.MX6DL, silicon rev 1.1
Console: colour dummy device 80x30
Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
ftrace: allocating 23648 entries in 70 pages
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x806d1848 - 0x806d18a0
Brought up 1 CPUs
SMP: Total of 1 processors activated (1581.05 BogoMIPS).
CPU: All CPU(s) started in SVC mode.
devtmpfs: initialized
pinctrl core: initialized pinctrl subsystem
regulator-dummy: no parameters
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
Use WDOG2 as reset source
syscon 20c8000.anatop: regmap [mem 0x020c8000-0x020c8fff] registered
vdd1p1: 800 <--> 1375 mV at 1125 mV
vdd3p0: 2800 <--> 3150 mV at 3000 mV
vdd2p5: 2000 <--> 2750 mV at 2425 mV
cpu: 725 <--> 1450 mV at 1150 mV
vddpu: 725 <--> 1450 mV at 1150 mV
vddsoc: 725 <--> 1450 mV at 1175 mV
syscon 20e0000.iomuxc-gpr: regmap [mem 0x020e0000-0x020e0037] registered
syscon 21bc000.ocotp-ctrl: regmap [mem 0x021bc000-0x021bffff] registered
hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 4 bytes.
imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
bio: create slab <bio-0> at 0
mxs-dma 110000.dma-apbh: initialized
i2c-core: driver [max17135] using legacy suspend method
i2c-core: driver [max17135] using legacy resume method
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
PTP clock support registered
imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
MIPI CSI2 driver module loaded
Advanced Linux Sound Architecture Driver Initialized.
cfg80211: Calling CRDA to update world regulatory domain
Switching to clocksource mxc_timer1
NET: Registered protocol family 2
TCP established hash table entries: 8192 (order: 4, 65536 bytes)
TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
TCP: Hash tables configured (established 8192 bind 8192)
TCP: reno registered
UDP hash table entries: 512 (order: 2, 16384 bytes)
UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
pureg-dummy: no parameters
imx6_busfreq busfreq.15: busfreq_probe: failed to get axi_sel_clk
imx6_busfreq: probe of busfreq.15 failed with error -2
Bus freq driver module loaded
VFS: Disk quotas dquot_6.5.2
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
fuse init (API version 7.22)
msgmni has been set to 1999
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
imx-weim 21b8000.weim: WEIM driver registered.
MIPI DSI driver module loaded
imx-sdma 20ec000.sdma: no iram assigned, using external mem
imx-sdma 20ec000.sdma: initialized
imx-sdma 20ec000.sdma: loaded firmware 1.1
Serial: IMX driver
2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX
console [ttymxc0] enabled
serial: Freescale lpuart driver
[drm] Initialized drm 1.1.0 20060810
[drm] Initialized vivante 1.0.0 20120216 on minor 0
brd: module loaded
loop: module loaded
lkdtm: No crash points registered, enable through debugfs
m25p80 spi32766.0: found mr25h256, expected m25p32
m25p80 spi32766.0: mr25h256 (32 Kbytes)
spi_imx 2008000.ecspi: probed
CAN device driver interface
libphy: fec_enet_mii_bus: probed
fec 2188000.ethernet eth0: registered PHC device 0
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
usbcore: registered new interface driver usb-storage
ci_hdrc ci_hdrc.0: doesn't support gadget
ci_hdrc ci_hdrc.0: EHCI Host Controller
ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1
ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
mousedev: PS/2 mouse device common for all mice
i2c-core: driver [isl29023] using legacy suspend method
i2c-core: driver [isl29023] using legacy resume method
snvs_rtc 20cc034.snvs-rtc-lp: rtc core: registered 20cc034.snvs-rtc-lp as rtc0
i2c /dev entries driver
i2c-core: driver [mag3110] using legacy suspend method
i2c-core: driver [mag3110] using legacy resume method
imx2-wdt 20bc000.wdog: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=0)
cpuidle: using governor ladder
cpuidle: using governor menu
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
usbcore: registered new interface driver ushc
sdhci-pltfm: SDHCI platform and OF driver helper
mmc0: no vqmmc regulator found
mmc0: no vmmc regulator found
mmc0: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA
mmc0: mmc_rescan_try_freq: trying to init card at 400000 Hz
mmc0: host does not support reading read-only switch. assuming write-enable.
mmc0: new high speed SD card at address 59b4
mmcblk0: mmc0:59b4 USD 1.87 GiB
(usually hangs here)
...
(but sometimes the boot continue in this way)
Unable to handle kernel paging request at virtual address afff0000
pgd = 80004000
[afff0000] *pgd=4ffcf801, *pte=00000000, *ppte=00000000
Internal error: Oops: 807 [#1] PREEMPT ARM
Modules linked in:
CPU: 0 PID: 1 Comm: swapper Not tainted 3.10.17+g232293e #14
task: a805a000 ti: a806c000 task.ti: a806c000
PC is at __memzero+0x24/0x80
LR is at 0x0
pc : [<80264cc4>] lr : [<00000000>] psr: 20000113
sp : a806dd6c ip : 00000000 fp : 00000000
r10: a80c4610 r9 : a806ddbc r8 : 00008000
r7 : 00000047 r6 : 8113b000 r5 : 08000000 r4 : aa500000
r3 : 00000000 r2 : 00000000 r1 : 0250ffc0 r0 : afff0000
Flags: nzCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment kernel
Control: 10c53c7d Table: 10004059 DAC: 00000015
Process swapper (pid: 1, stack limit = 0xa806c230)
Stack: (0xa806dd6c to 0xa806e000)
dd60: 80015fec 00000001 08000000 8113b000 08000000
dd80: 00000047 00008000 a806ddbc 80016720 fffffffe 00000000 08000000 00000000
dda0: 00000000 00000000 a82a9b94 80016960 803e6be4 00000001 80bcbea0 00000000
ddc0: 00000047 a82a9b94 08000000 a80c4610 000000d0 803e6be4 80b2fb40 80016c1c
dde0: 00000047 00000000 803e6be4 800b1158 00000000 8030914c a82a9b80 80b75d30
de00: a80c4610 a80c4610 a80c4600 a82a9b90 80b23814 803e6be4 a82a9b90 80110e6c
de20: 00200200 00001ebe a82a9a40 a82a9b40 a806de60 80111058 00000000 a82a9a40
de40: 00000000 a82a9b40 a80c3e00 80111a68 00000000 800b04e0 a82a9a80 a82a9a90
de60: a80c3e00 00000000 a80c4610 80be36a0 a80c4610 00000000 80b75d44 80b81340
de80: 80b23814 80b2fb40 00000000 80307d5c 80307d44 80306adc 00000000 a80c4610
dea0: 80b75d44 a80c4644 00000000 80306cc8 00000000 80b75d44 80306c3c 80304fe0
dec0: a804234c a80c16b0 80b75d44 a829ad80 80b649e0 803062a0 80a86a60 80267fdc
dee0: 80b75d44 80b75d44 00000006 80b81340 80b81340 803072d0 80b3bea8 00000006
df00: 80b81340 80b81340 80b81340 80008744 000000ab 80040508 00000000 a806c010
df20: 80a7f5f8 80ad0d28 00000006 00000006 8003fd74 8003fdcc 00000000 80b3bea8
df40: 00000006 80b81340 80b81340 80afd480 000000ab 80b2fb40 80b2fb34 80afdb68
df60: 00000006 00000006 80afd480 7a5dcff3 ebdbb65f 7567aef9 5f7fb2ef 00000000
df80: 8056e6cc 00000000 00000000 00000000 00000000 00000000 00000000 8056e6d4
dfa0: 00000000 00000000 8056e6cc 8000e118 00000000 00000000 00000000 00000000
dfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
dfe0: 00000000 00000000 00000000 00000000 00000013 00000000 00000000 00000001
Code: e52de004 e1a0c002 e1a0e002 e2511040 (a8a0500c)
---[ end trace 993561f6a7d64d56 ]---
Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b
--
Marco
解決済! 解決策の投稿を見る。
Hi Igor,
I solved and now I am able to boot a kernel derived from iMX6DLSABRE.
The problem was caused by bad regulators settings like vmmc-supply = <®_3p3v> in the DeviceTree.
Thank you very much for your support.
--
Marco
Hi Marco
for Solo one needs to use imx6dl.dtb, since i.MX6Solo
is the same as DL only with one core, refer to p.3 attached document.
Also for new board one needs to run DDR test and update DDR settings
in .cfg file (like mx6q_4x_mt41j128.cfg)
i.MX6 DDR Stress Test Tool V1.0.3
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
your instrunctions are not clear. Are they related to SABREAUTO?
I expected to start cloning a SABLESD.
If I do as you said, the kernel doesn't boot at all and immediately reset the board.
make imx_v7_defconfig
make -j4 uImage LOADADDR=0x10008000
make imx6dl-sabresd.dtb
U-Boot 2015.01 (Feb 27 2015 - 17:44:58)
CPU: Freescale i.MX6SOLO rev1.1 at 792 MHz
CPU: Temperature 22 C
Reset cause: POR
Board: MX6-SabreQ - *** Version (0.2.0) ***
I2C: ready
DRAM: 1 GiB
PMIC: PFUZE100 ID=0x10
MMC: 0
FSL_SDHC: 0, FSL_SDHC: 1
...
tftp ${loadaddr} uImage
tftp ${fdt_addr} imx6
bootm ${loadaddr} - ${fdt_addr}
...
Bytes transferred = 39589 (9aa5 hex)
## Booting kernel from Legacy Image at 12000000 ...
Image Name: Linux-3.10.17+g232293e
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 5739888 Bytes = 5.5 MiB
Load Address: 10008000
Entry Point: 10008000
Verifying Checksum ... OK
## Flattened Device Tree blob at 18000000
Booting using the fdt blob at 0x18000000
Loading Kernel Image ... OK
Loading Device Tree to 4f556000, end 4f562aa4 ... OK
Starting kernel ...
(here board reset)
Hi Marco
for new custom board had you run DDR test ?
After that one needs to rebuild Uboot with updated DDR settings
in Uboot .cfg file (like mx6q_4x_mt41j128.cfg)
i.MX6 DDR Stress Test Tool V1.0.3
~igor
Hi Igor,
we did run DDR test.
U-boot 2015 boot perfectly, MMC, fatload, TFTP works.
Linux 3.10.17 derived from iMX6Q-SABRE boots as I showed in my first post above.
There must be something more subtle to define in the DeviceTree perhaps.
Thank you
--
Marco
Hi Marco
one can try Demo images
L3.10.17_1.0.2_iMX6QDLS_BUNDLE : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo Linux Binary Demo Files
also one can try ldo configuration: imx6dl-sabresd-ldo, for auto - imx6dl-sabreauto.
~igor
Hi Igor,
I downloaded fsl-L3.10.17_1.0.2_iMX6QDLS_Bundle.
I have noticed that it use u-boot-2013.04 so I downloaded it and rebuilt from scratch
u-boot imx_v2013.04_3.10.17_1.0.0_ga
and
make mx6solosabresd_config
Configuring for mx6solosabresd - Board: mx6qsabresd, Options:
IMX_CONFIG=board/freescale/mx6qsabresd/mx6solo_4x_mt41j128.cfg,
MX6SOLO,DEFAULT_FDT_FILE="imx6dl-sabresd.dtb",DDR_MB=512,SYS_USE_SPINOR,SYS_NOSMP="nosmp"
Now I booted it
U-Boot 2013.04-04986-g06dd4f7-dirty (Mar 03 2015 - 15:23:22)
CPU: Freescale i.MX6SOLO rev1.1 at 792 MHz
CPU: Temperature 43 C, calibration data: 0x5a151069
Reset cause: POR
Board: MX6Q/SDL-SabreSD
I2C: ready
DRAM: 512 MiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
Then I load my kernel from MMC1
Booting Linux on physical CPU 0x0
Linux version 3.10.17+g232293e (koan@amonra) (gcc version 4.8.2 (GCC) ) #47 SMP PREEMPT Mon Mar 2 11:43:53 CET 2015
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: Freescale i.MX6 Quad/DualLite (Device Tree), model: Freescale i.MX6 Quad SABRE Smart Device Board
cma: CMA: reserved 320 MiB at 1c000000
Memory policy: ECC disabled, Data cache writealloc
PERCPU: Embedded 9 pages/cpu @812f1000 s12992 r8192 d15680 u36864
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 130048
Kernel command line: noinitrd console=ttymxc0,115200
PID hash table entries: 2048 (order: 1, 8192 bytes)
Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
Memory: 512MB = 512MB total
Memory: 176068k/176068k available, 348220k reserved, 0K highmem
...
usbcore: registered new interface driver ushc
sdhci-pltfm: SDHCI platform and OF driver helper
mmc0: no vqmmc regulator found
mmc0: no vmmc regulator found
mmc0: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA
mmc0: mmc_rescan_try_freq: trying to init card at 400000 Hz
mmc0: host does not support reading read-only switch. assuming write-enable.
mmc0: new high speed SD card at address 59b4
mmcblk0: mmc0:59b4 USD 1.87 GiB
mmcblk0: p1 p2
Galcore version 4.6.9.9754
(here hangs)
What doed the new line "Galcore version 4.6.9.9754" mean?
TIA
Marco,
The Galcore hang happens because you use imx6dl-sabredsd.dtb instead of imx6dl-sabresd-ldo.dtb.
Regards,
Fabio Estevam
The weird thing is that I noticed that Yocto Project build a solosabre system using the DLsabre Devicetree.
In my case whenever I use the DL the kernel doesn't boot and the system immediately reboot, if I use the Quad it boot as shown above.
Hi Marco
had you configured properly DDR in Uboot, because from your logs:
U-Boot 2015.01 (Feb 27 2015 - 17:44:58) --> DRAM: 1 GiB
u-boot imx_v2013.04_3.10.17_1.0.0_ga ---> DRAM: 512 MiB
also please try imx6dl-sabresd-ldo.dtb, as was suggested
It may be recommended to try minimal build (without GPU/VPU support).
Best regards
igor
Hi Igor,
you are right. I noticed that and that's the reason why I moved from u-boot-2015.01 to u-boot-2013.04.
I don't understand why u-boot-2015.01 has this weird behaviour despite the same settings I am using.
However I will focus on the Freescale suggested version u-boot-2013.04.
I ran the DDR test ad you suggested and I found a slightly difference in these registers only (the ones provided by DDR test) but the final result is the same.
DATA 4, 0x021b080c, 0x0047004B // MMDC_MPWLDECTRL0
DATA 4, 0x021b0810, 0x003B003F // MMDC_MPWLDECTRL1
DATA 4, 0x021b083c, 0x423C023C // MPDGCTRL0 PHY0
DATA 4, 0x021b0840, 0x022C022C // MPDGCTRL1 PHY0
DATA 4, 0x021b0848, 0x44464648 // MPRDDLCTL PHY0
DATA 4, 0x021b0850, 0x34362C2E // MPWRDLCTL PHY0
After u-boot-2013.04 rebuild, the result running my kernel 3.10.17 without "MXC Vivante GPU support" is always the same:
...
kjournald starting. Commit interval 5 seconds
(freezes here)
About the imx6dl-sabresd-ldo.dtb, as I said, using it the kernel immediately reboots.
Is it normal?
Are you sure I need to use DUALLITE kernel system for the SOLO board?
> fatload mmc 1:1 0x18000000 imx6dl-sabresd-ldo.dtb
reading imx6dl-sabresd-ldo.dtb
47956 bytes read in 20 ms (2.3 MiB/s)
> bootm 0x12000000 - 0x18000000
## Booting kernel from Legacy Image at 12000000 ...
Image Name: Linux-3.10.17+g232293e
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 5659696 Bytes = 5.4 MiB
Load Address: 10008000
Entry Point: 10008000
Verifying Checksum ... OK
## Flattened Device Tree blob at 18000000
Booting using the fdt blob at 0x18000000
Loading Kernel Image ... OK
OK
Using Device Tree in place at 18000000, end 1800eb53
Starting kernel ...
(reboot here)
Hi Marco
refer to attached document
2.1 Boot Loader
i.MX 6Solo SABRE-AI:
• u-boot-imx6solosabreauto.imx (SD/MMC)
• u-boot-imx6solosabreauto_spi-nor.imx (SPI-NOR)
• u-boot-imx6solosabreauto_eim-nor.imx (Parallel NOR)
• u-boot-imx6solosabreauto_nand.imx (NAND)
p.3
i.MX 6DualLite SABRE-AI, i.MX 6Solo SABRE-AI:
• uImage_imx_v7_defconfig
• uImage-imx6dl-sabreauto.dtb
• uImage-imx6dl-sabreauto-ecspi.dtb
• uImage-imx6dl-sabreauto-gpmi-weim.dtb
• uImage-imx6dl-sabreauto-flexcan1.dtb
~igor
Hi Igor,
the HW engineer has a doubt.
In this case I have a board mounting i.MXSOLO and 32bit DDR3 (2x MT41K128M16) and a total of 512MB
Is this design supported by the CPU?
Hi Marco
it is supported, otherwise you would not
run Uboot. Freescale reference designs
are i.MX6DL,i.MX6Q with 64bits DDR3.
However for i.MX6Solo one needs to set 32bit width
in dcd header (DDR initialization). 512MB is too few
for graphic/video - probably you will need to tweak linux
memory settings. It may be interesting to look at attached
document about linux Solo differencies.
Recommended to check that linux does not try
to run ddr at 532MHz (Solo supports up to 400MHz).
~igor
H Igor,
the document you provided contains some interesting patches reference (ENGR*), however looks like they are related to a i.MX6DL starting point.
Unfortunately, as I said I had to use imx6q-sabresd-ldo.dtb (or imx6q-sabresd.dtb) because the imx6dl-sabresd-ldo.dtb reset immediately my board.
Do you have any hint on that?
Hi Marco
what design was used as reference for that board ?
What PMIC ?
Since board is reset, I am not sure that your board is hardware
healthy regarding DDR and power. So I would suggest
to try any linux to check it. Uboot is quite tolerant to DDR errors,
while linux - not. Also uboot does not use power management and
cpu-freq (linux) driver.
~igor
Hi Igor,
this design was created following your reference design SPF-27516_C3 which uses a i.MX6 Quad.
The PMIC is MMPF0100F0EP.
In the schematic we only removed the circuit parts regarding the second RAM bus leaving the connections for the remaining bus exactly the same as in you design.
TIA
Hi Marco
could you also check if all differencies were implemented
as required by sect.4.1 Connection differences
AN4397 Common Hardware Design for i.MX 6Dual/6Quad and i.MX 6Solo/6DualLite
Best regards
igor
This is our DDR3 configuration. It uses one CS only and in your doc AN4397 is not listed this configuration.
Is it correct?
Thanks
I think it is correct.
Also could you check that capacitors at _CAP nodes, NVCC_PLL_OUT
have values recommended by latest Design Check List
HW Design Checking List for i.MX6DQSDL
regarding last hanging case with uboot 2013 :
Galcore version 4.6.9.9754
(here hangs)
please add maxcpus=1 to kernel command line and check similar issue on link below
kernel hangs or fails to allocate CMA in galcore with i.MX Solo Sabre
~igor
Hi Igor,
I solved and now I am able to boot a kernel derived from iMX6DLSABRE.
The problem was caused by bad regulators settings like vmmc-supply = <®_3p3v> in the DeviceTree.
Thank you very much for your support.
--
Marco