Latest uboot source missing sabre board and config files

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Latest uboot source missing sabre board and config files

3,832 Views
sriramchadalava
Contributor III

I followed the instructions in the Freescale Android Users Guide Rev jb4.2.2_1.0.0-GA to pull latest uboot source.

However, when I tried building it, it failed.

ram@ram-Latitude-E6520:~/Prevas/Android_porting/Freescale/imx6/4.2.2/myandroid/bootable/bootloader/uboot-imx$ make mx6q_sabresd_android_config

awk '(NF && $1 !~ /^#/) { print $1 ": " $1 "_config; $(MAKE)" }' boards.cfg > .boards.depend

make: *** No rule to make target `mx6q_sabresd_android_config'.  Stop.

make: *** [mx6q_sabresd_android_config] Error 1

When I compared this version of uboot source with the uboot source I pulled with 4.0.4 Freescale release, I found these files missing:


./board/freescale/mx6q_sabrelite

./board/freescale/mx6q_sabrelite/mx6q_sabrelite.c

./board/freescale/mx6q_sabrelite/lowlevel_init.S

./board/freescale/mx6q_sabrelite/config.mk

./board/freescale/mx6q_sabrelite/u-boot.lds

./board/freescale/mx6q_sabrelite/Makefile

./board/freescale/mx6q_sabrelite/flash_header.S

./board/freescale/mx6q_sabresd

./board/freescale/mx6q_sabresd/libmx6q_sabresd.a

./board/freescale/mx6q_sabresd/lowlevel_init.S

./board/freescale/mx6q_sabresd/mx6q_sabresd.c

./board/freescale/mx6q_sabresd/config.mk

./board/freescale/mx6q_sabresd/u-boot.lds

./board/freescale/mx6q_sabresd/.depend

./board/freescale/mx6q_sabresd/Makefile

./board/freescale/mx6q_sabresd/flash_header.S

./board/freescale/mx6q_sabreauto

./board/freescale/mx6q_sabreauto/lowlevel_init.S

./board/freescale/mx6q_sabreauto/mx6q_sabreauto.c

./board/freescale/mx6q_sabreauto/config.mk

./board/freescale/mx6q_sabreauto/u-boot.lds

./board/freescale/mx6q_sabreauto/Makefile

./board/freescale/mx6q_sabreauto/flash_header.S

./include/configs/mx6solo_sabreauto_weimnor_mfg.h

./include/configs/mx6q_sabresd_iram.h

./include/configs/mx6dl_sabreauto_mfg.h

./include/configs/mx6dl_sabresd_android.h

./include/configs/mx6solo_sabreauto.h

./include/configs/mx6solo_sabreauto_mfg.h

./include/configs/mx6dl_sabreauto_spi-nor.h

./include/configs/mx6solo_sabresd_android.h

./include/configs/mx6q_sabresd_android.h

./include/configs/mx6q_sabreauto_spi-nor_mfg.h

./include/configs/mx6q_sabrelite_mfg.h

./include/configs/mx6q_sabreauto_nand_mfg.h

./include/configs/mx6q_sabreauto_mfg.h

./include/configs/mx6dl_sabreauto_weimnor.h

./include/configs/mx6q_sabreauto_weimnor.h

./include/configs/mx6solo_sabreauto_nand_mfg.h

./include/configs/mx6q_sabrelite.h

./include/configs/mx6solo_sabresd.h

./include/configs/mx6solo_sabreauto_spi-nor_mfg.h

./include/configs/mx6dl_sabreauto_nand_mfg.h

./include/configs/mx6dl_sabreauto_spi-nor_mfg.h

./include/configs/mx6dl_sabresd.h

./include/configs/mx6q_sabresd_mfg.h

./include/configs/mx6solo_sabreauto_spi-nor.h

./include/configs/mx6q_sabreauto_nand.h

./include/configs/mx6dl_sabreauto_nand.h

./include/configs/mx6dl_sabresd_mfg.h

./include/configs/mx6dl_sabreauto_weimnor_mfg.h

./include/configs/mx6q_sabresd.h

./include/configs/mx6dl_sabreauto.h

./include/configs/mx6q_sabreauto_spi-nor.h

./include/configs/mx6q_sabreauto_weimnor_mfg.h

./include/configs/mx6solo_sabreauto_nand.h

./include/configs/mx6q_sabreauto.h

./include/configs/mx6q_sabrelite_android.h

./include/configs/mx6solo_sabreauto_weimnor.h

Is this something broken on the jb4.2.2_1.0.0-ga branch? If so, how do I ask or notify the code maintainers?


Thanks


Labels (3)
5 Replies

2,105 Views
lily_zhang
NXP Employee
NXP Employee

I checked U-boot source codes in http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/tree/board/freescale?id=jb4.2.2_1.0.0-ga . The board files you mentioned to be missing are still here. How did you get U-boot source codes?

2,105 Views
sriramchadalava
Contributor III

Hi Xiaoli,

  Thanks for the reply.

  I would like to add to my previous post that board.cfg has no entries for these boards.

   Just followed the following instructions from the Freescale Android User's Guide document(Rev jb4.2.2_1.0.0-GA 05/2013).

$ git clone git://git.freescale.com/imx/uboot-imx.git uboot-imx

$ cd uboot-imx

$ git checkout jb4.2.2_1.0.0-ga

I also tried an http clone (not that should make a difference)

Interesting thing is that ALL the files and relevant entries in board.cfg ARE available from git://github.com/Freescale/u-boot-imx.git.

0 Kudos
Reply

2,105 Views
kobyhershkovitz
Contributor I

I had the same problem, and it turned out I was on the master branch instead of the  jb4.2.2_1.0.0-ga branch.

after switching to the correct branch the build was OK.

0 Kudos
Reply

2,105 Views
YixingKong
Senior Contributor IV

Sriram, if your questions had been aswered, please click Correct Answer/Helpful Answer.

Thanks,

Yixing

0 Kudos
Reply

2,105 Views
lily_zhang
NXP Employee
NXP Employee

Just now i tried the following steps and the build is OK:

$ git clone git://git.freescale.com/imx/uboot-imx.git uboot-imx

$ cd uboot-imx

$ git checkout jb4.2.2_1.0.0-ga

$ make ARCH=arm CROSS_COMPILE=/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-none-linux-gnueabi- mx6q_sabresd_android_config

$ make ARCH=arm CROSS_COMPILE=/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-none-linux-gnueabi-