Latest kernel version supported by IMX.50

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Latest kernel version supported by IMX.50

Jump to solution
2,773 Views
lyfsci
Contributor III

Hi Experts,

What is the latest kernel version supported for the IMX50 EVK ?

When I tried to downloaded the source it shows like 2.6 versions of kernel. Is it the one available or any other software SDK's containing the 3.2 and above kernel versions ?

0 Kudos
Reply
1 Solution
2,654 Views
igorpadykov
NXP Employee
NXP Employee

Hi lyf

latest Freescale official release

L2.6.35__11.04_ER_SOURCE : Linux 2.6.35 Source Code Files and documentation 2011.04.

Size (K): 732535 Format: gz Rev #: 2011.04 Modified: 7/7/2011


i.MX508 Processors|Integrated EPD|Freescale


Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
2,655 Views
igorpadykov
NXP Employee
NXP Employee

Hi lyf

latest Freescale official release

L2.6.35__11.04_ER_SOURCE : Linux 2.6.35 Source Code Files and documentation 2011.04.

Size (K): 732535 Format: gz Rev #: 2011.04 Modified: 7/7/2011


i.MX508 Processors|Integrated EPD|Freescale


Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,654 Views
lyfsci
Contributor III

Hi,

Is there any guidelines to port the latest kernel support for the IMX50 ?

0 Kudos
Reply
2,654 Views
igorpadykov
NXP Employee
NXP Employee

I think no.