Latest kernel version supported by IMX.50

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Latest kernel version supported by IMX.50

ソリューションへジャンプ
2,788件の閲覧回数
lyfsci
Contributor III

Hi Experts,

What is the latest kernel version supported for the IMX50 EVK ?

When I tried to downloaded the source it shows like 2.6 versions of kernel. Is it the one available or any other software SDK's containing the 3.2 and above kernel versions ?

0 件の賞賛
返信
1 解決策
2,669件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi lyf

latest Freescale official release

L2.6.35__11.04_ER_SOURCE : Linux 2.6.35 Source Code Files and documentation 2011.04.

Size (K): 732535 Format: gz Rev #: 2011.04 Modified: 7/7/2011


i.MX508 Processors|Integrated EPD|Freescale


Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,670件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi lyf

latest Freescale official release

L2.6.35__11.04_ER_SOURCE : Linux 2.6.35 Source Code Files and documentation 2011.04.

Size (K): 732535 Format: gz Rev #: 2011.04 Modified: 7/7/2011


i.MX508 Processors|Integrated EPD|Freescale


Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,669件の閲覧回数
lyfsci
Contributor III

Hi,

Is there any guidelines to port the latest kernel support for the IMX50 ?

0 件の賞賛
返信
2,669件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

I think no.