Latest Uboot and Kernel Version Supported for IMX6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Latest Uboot and Kernel Version Supported for IMX6

4,761 次查看
rajniks
Contributor I

I have a LTIB L3.0.35_4.1.0 installed on a Unbutu 12.04 Linux host and version of Uboot and Kernel supported are given below

linux-3.0.35

uboot-2009.08

I wanted to know if there is a updated version supported now and if yes how can get the sourcecode and relevant patch files to update my ltib as well.

标签 (4)
标记 (4)
0 项奖励
回复
6 回复数

2,324 次查看
rajniks
Contributor I

I have followed Yocto User manual and downloaded it on my computer but it needs lot of resources and I have not been to able to build the default u-boot itself. LTIB was comparatively much lighter. I have LTIB working installation. Just wanted to know if Freescale supports both or I need to move to Yocto.

As of now I have not been successful with Yocto.

0 项奖励
回复

2,324 次查看
LuisCasado
NXP Employee
NXP Employee

Hello,

Freescale has moved the Linux BSP to Yocto.

Linux 3.10.17

o   Source Code Download Steps Documentation and Demo Images

Documentation:

o   Linux 3.10.17 BSP & MM Bundle

Also, you can find the latest Kernel and u-boot in the git.

http://git.freescale.com/git/

Luis

0 项奖励
回复

2,324 次查看
shabeerbadarudh
Contributor IV

Hi Luis ,

I downloaded both the source code and documents. But i am doubting about the header files.. In the Linux reference manual the header file location is ' <Yocto_BuildDir>/linux/arch/arm/plat-mxc/include/mach'. But in the 'plat-mxc' folder is missing in linux BSP. Where is the header file location in 3.10.17.

Regards

Shabeer

0 项奖励
回复

2,324 次查看
tonyzheng
NXP Employee
NXP Employee

Hi,Shabeer

In 3.10.17, you can try to find it in arch/arm/mach-imx.

0 项奖励
回复

2,324 次查看
rajniks
Contributor I

Hi Luis,

I tried to download through the git as discussed the PDF document "Freescale_Yocto_Project_User's_Guide" but looks like my organization has blocked git access. Is there any workaround to set this up?

0 项奖励
回复

2,324 次查看
tonyzheng
NXP Employee
NXP Employee

Hello,

You can use proxy server to download it. it need that you consult your organization's IT service and ask for proxy server IP.

0 项奖励
回复