Latest Pin Tools includes support for IMX6ULL?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Latest Pin Tools includes support for IMX6ULL?

ソリューションへジャンプ
2,153件の閲覧回数
djregan
Contributor III

Hi everyone, Just double-checking...

Does the latest Pin Tools release include support for IMX6ULL?

Reason 'why?' I ask: See NXP Pin Tools Download page here...

https://www.nxp.com/pages/pins-tool-for-i.mx-application-processors:PINS-TOOL-IMX?

The current list of supported processors excludes the IMX6ULL, but does mention...

Supported Devices

i.MX6QP: i.MX 6QuadPlus Processor - Quad-Core, High-Performance, Advanced 3D Graphics, HD Video, Advanced Multimedia, ARM® Cortex®-A9 Core
i.MX6Q: i.MX 6Quad Processors - High-Performance, 3D Graphics, HD Video, Arm Cortex-A9 Core
i.MX6DP: i.MX 6DualPlus Processor - Dual-Core, High-Performance, Advanced 3D Graphics, HD Video, Advanced Multimedia, Arm® Cortex®-A9 Core
i.MX6D: i.MX 6Dual Processors - Dual-Core, 3D Graphics, HD Video, Multimedia, ARM Cortex-A9 Core
i.MX6DL: i.MX 6DualLite Processors – Dual-Core, 3D Graphics, HD Video, Arm Cortex-A9 Core
i.MX6S: i.MX 6Solo Processors – Single-Core, Multimedia, 3D Graphics, ARM Cortex-A9 Core
i.MX6SX: i.MX 6SoloX Processors - Heterogeneous Processing with ARM® Cortex®-A9 and Cortex-M4 cores
i.MX6SL: i.MX 6SoloLite Processors – Single-Core, Low-Power, EPD Controller, Arm Cortex-A9 Core
i.MX6UL: i.MX 6UltraLite Processor - Low-power, secure, Arm® Cortex®-A7 Core
i.MX7D: i.MX 7Dual Processors - Heterogeneous Processing with dual Arm® Cortex®-A7 cores and Cortex-M4 core
i.MX7S: i.MX 7Solo Processors - Heterogeneous Processing with Arm® Cortex®-A7 and Cortex-M4 cores
i.MX6SLL: i.MX 6SLL Processors - Single-Core Processor with ARM® Cortex®-A9 Core
i.MX-RT1050: i.MX RT1050 Crossover Processor with Arm® Cortex®-M7 core

Is omission of IMX6ULL intended?

Thanks much in advance!

Best Regards,

--DJ Regan

ラベル(1)
タグ(2)
1 解決策
2,012件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  the recent Pins for i.MX (version 4) supports i.MX 6ULL.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
2,013件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  the recent Pins for i.MX (version 4) supports i.MX 6ULL.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,012件の閲覧回数
djregan
Contributor III

Awesome news! Appreciate it Yuri! --DJ

0 件の賞賛
返信