LVDS resolution problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LVDS resolution problem

1,262件の閲覧回数
kikimorisato
Contributor II

BSP: fsl-community-bsp (fido branch)

Kernel Version: 3.14.28

Board: SabreSD (mx6q)

LCD: Innolux 1024x600 LVDS

no X11 (frame buffer use)

Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk2p2 rootwait rw video=mxcfb0:dev=ldb,1024x600M@60

u-boot lcd resolution is OK

but linux lcd resolution is always 1024x768

for examples

1. gstreamer

gst-launch v4l2src device=/dev/video0  ! 'video/x-raw-yuv, format=(fourcc)UYVY' ! mfw_isink

than ==>

MAX resolution 1024x768

MFW_GST_ISINK_PLUGIN 4.0.3 build on Apr 20 2015 18:43:18.

Setting pipeline to PAUSED ...tw6869 0000:01:00.0: vch0 std NTSC (M)

tw6869 0000:01:00.0: vch0 fps 29

tw6869 0000:01:00.0: DMA 0 ON

Pipeline is live and does not need PREROLL ...

Setting pipeline to PLAYING ...

New clock: GstSystemClock

hwbuf allocator zone(692224) created

VS0 created. in fmt[YUYV] win(0,0-720,480:720x480) out win(0,0-1024,768:1024x768)

set deinterlace mode 0

2. QT5.4.1 resizeGL (from system width height)

W = 1024

H = 768

---------------------------------------------------------------------------------------------------------------------------------------------------------------------------------

how can i change linux LVDS resolution

---------------------------------------------------------------------------------------------------------------------------------------------------------------------------------


and max11801 touch device resolution is 1024x768 too

ラベル(1)
タグ(2)
0 件の賞賛
返信
0 返答(返信)