LVDS panel display corruption

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LVDS panel display corruption

1,183 Views
wimvanloocke
Contributor I

see https://community.freescale.com/thread/320314#comments

processor

Freescale i.MX6SOLO rev1.1 at 792 MHz

It seems this problem is not resolved in kernel 3.10.17.   The driver has changed quite a bit, so i don't know if this problem was taken along in the redesign or just not taken up.

Labels (1)
0 Kudos
Reply
1 Reply

1,011 Views
igorpadykov
NXP Employee
NXP Employee

Hi vim

3.10.17 is quite old kernel and I am not sure that new patches are

released for it. According to link activity 17.07.2014 15:31, Jeff Horn

produced patch, you can ask it from him. In general recommended to

use latest kernel

Board Support Packages (29)

L3.14.52_1.1.0_MX6QDLSOLO (REV L3.14.52_1.1.0)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply