LVDS panel display corruption

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LVDS panel display corruption

1,199件の閲覧回数
wimvanloocke
Contributor I

see https://community.freescale.com/thread/320314#comments

processor

Freescale i.MX6SOLO rev1.1 at 792 MHz

It seems this problem is not resolved in kernel 3.10.17.   The driver has changed quite a bit, so i don't know if this problem was taken along in the redesign or just not taken up.

ラベル(1)
0 件の賞賛
返信
1 返信

1,027件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi vim

3.10.17 is quite old kernel and I am not sure that new patches are

released for it. According to link activity 17.07.2014 15:31, Jeff Horn

produced patch, you can ask it from him. In general recommended to

use latest kernel

Board Support Packages (29)

L3.14.52_1.1.0_MX6QDLSOLO (REV L3.14.52_1.1.0)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信