LVDS format in the device tree

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LVDS format in the device tree

1,613 Views
greeranjunk
Contributor III

hi

i am connecting my imx8m-mini to a custom LVDS screen. i changed the device tree LVDS timing but still did not get a picture. at the end i change the lvds-format value from 1 to 2 and it fixed the LVDS output. I tried to find information about the lvds-format values but could not find any. could you tell me what are the value options and what they mean

thanks

0 Kudos
Reply
2 Replies

1,542 Views
greeranjunk
Contributor III

my question was from lack of knowledge. the LVDS is standard and is configured by the resulotion. i googled the lvds 720p resolution configuration and added it to the device tree and everything works well

thanks

0 Kudos
Reply

1,542 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi ran gree,

i.MX8M MINI doesn't support LVDS interface, but MIPI DSI interface for display, which supports 1080P resolution.

Hope the information is helpful to you.

Have a nice day!

B.R,

Weidong

0 Kudos
Reply