LVDS format in the device tree

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LVDS format in the device tree

1,597件の閲覧回数
greeranjunk
Contributor III

hi

i am connecting my imx8m-mini to a custom LVDS screen. i changed the device tree LVDS timing but still did not get a picture. at the end i change the lvds-format value from 1 to 2 and it fixed the LVDS output. I tried to find information about the lvds-format values but could not find any. could you tell me what are the value options and what they mean

thanks

0 件の賞賛
返信
2 返答(返信)

1,526件の閲覧回数
greeranjunk
Contributor III

my question was from lack of knowledge. the LVDS is standard and is configured by the resulotion. i googled the lvds 720p resolution configuration and added it to the device tree and everything works well

thanks

0 件の賞賛
返信

1,526件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi ran gree,

i.MX8M MINI doesn't support LVDS interface, but MIPI DSI interface for display, which supports 1080P resolution.

Hope the information is helpful to you.

Have a nice day!

B.R,

Weidong

0 件の賞賛
返信