LVDS display problem with kernel 3.14.28

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LVDS display problem with kernel 3.14.28

Jump to solution
5,832 Views
ivandrobyshevsk
Contributor II

I'm trying to add support for LVDS display to i.MX6DL board running 3.14.28 kernel, but the picture is distorted. See attached photos for details (in boot screen photo dark areas are supposed to be solid black).

The same display works fine with kernel imx_4.1.15_2.0.0_ga, but unfortunately there's a requirement to make it work with 3.14.28 kernel.

I've used exactly the same relevant DT nodes from 4.1.15 kernel (attached in a fido_display.dts file).

What is strange: setting resolution to 1920x1080 (proper/desired resolution is 800x480) and enabling split mode fixes the picture (see fbtest_ok.JPG), but it doesn't fit the display.

Any suggestions as to where to look: missing commit(s) to one of IPU drivers, DT properties, etc?

Also what kind of setting mismatch could produce picture distortion we are observing?

Thanks!

Labels (3)
Tags (2)
0 Kudos
Reply
1 Solution
5,749 Views
ivandrobyshevsk
Contributor II

For whatever reason, clock speed had to be set two times faster compared to kernel 4.1.15. With higher speed picture looks good again.

View solution in original post

0 Kudos
Reply
2 Replies
5,750 Views
ivandrobyshevsk
Contributor II

For whatever reason, clock speed had to be set two times faster compared to kernel 4.1.15. With higher speed picture looks good again.

0 Kudos
Reply
5,749 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ivan

one can check if recommended LDB Clock Switch Procedure was implemented as

recommended by EB821

https://www.nxp.com/docs/en/engineering-bulletin/EB821.pdf 

Also one can try official nxp bsps described on

https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/i.mx-6ser...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply