LVDS display porting documents

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LVDS display porting documents

2,724件の閲覧回数
hailiu
Contributor IV

Dear community,

Are there documents or examples to describe  steps to porting LVDS display on imx6s/dl for a customer display with resolution 1024x768. I read through imx_reference_manual for linux-5.10.9 and it says the lvds driver is in driver/video/fbdev/mxc/imx_lvds.c and driver/gpu/drm/imx_ldb.c, but I can only find the second file. The other thing is that the node mxfb1 in device tree is disabled, Do I need to enable it? 

 

thank you,

Hai

0 件の賞賛
返信
2 返答(返信)

2,717件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Hai

 

one can look at Chapter 12 Connecting LVDS Panel   i.MX Porting Guide​

and example

https://community.nxp.com/t5/i-MX-Processors/How-to-change-SABRE-SD-screen-resolution-in-LOLLIPOP-5-...

 

Best regards
igor

 

0 件の賞賛
返信

2,700件の閲覧回数
hailiu
Contributor IV

thank you,

I will go through the documents and see.

 

Hai

0 件の賞賛
返信