LVDS display is not working in IMX custom board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LVDS display is not working in IMX custom board

1,901 次查看
ashokp
Contributor I

Hi All,

 

I am using IMX6 based custom board and running kitkat from freescale. The kernel version is 3.0.35.

 

The HDMI and LCD displays are working fine  but LVDS display is not working fine. Please let me know if any issues in the code changes.

 

Below i copied the fb structure for your reference. Also attached my board file for your reference

 

static struct ipuv3_fb_platform_data sabresd_fb_data[] = {

        { /*fb0*/

        .disp_dev = "hdmi",

        .interface_pix_fmt = IPU_PIX_FMT_RGB24,

        .mode_str = "1920x1080M@60",

        .default_bpp = 24,

        .int_clk = false,

        .late_init = false,

        }, {

        .disp_dev = "lcd",

        .interface_pix_fmt = IPU_PIX_FMT_RGB24,

        .mode_str = "CLAA-WVGA",

        .default_bpp = 24,

        .int_clk = false,

        .late_init = false,

        }, {

        .disp_dev = "ldb",

        .interface_pix_fmt = IPU_PIX_FMT_RGB666,

//        .mode_str = "LDB-XGA",

        .default_bpp = 24,

        .int_clk = false,

        .late_init = false,

        },

};

 

 

 

static struct fsl_mxc_ldb_platform_data ldb_data = {

        .ipu_id = 0,   // ASHOK

        .disp_id = 0,

        .ext_ref = 1,

        .mode = LDB_SEP1,

        .sec_ipu_id = 0,

        .sec_disp_id = 0,

};

 

Thanks,

P.Ashok

Original Attachment has been moved to: board-mx6q_sabresd.c.zip

标签 (3)
0 项奖励
回复
3 回复数

1,257 次查看
alejandrolozan1
NXP Employee
NXP Employee

Hi,

I skimmed through the file and it seems to be fine.

I would start changing the IPU ids and see if there is any difference.

0 项奖励
回复

1,257 次查看
alejandrolozan1
NXP Employee
NXP Employee

Hi,

Have you tried with a different IPU id? Do you want the LVDS1 to be your primary display?

Regards,

Alejandro

0 项奖励
回复

1,257 次查看
ashokp
Contributor I

Hi Alejandro,

Yes i  want LVDS1 to be a primary display. Please let me know is anything wrong in my my board file

Thanks

P.Ashok

0 项奖励
回复