LVDS and RGB Displays Design

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LVDS and RGB Displays Design

4,200件の閲覧回数
rajniks
Contributor I

Most of the displays both LVDS and RGB that I have seen have a very stringent requirement that display signals and function signals need to high impedance or low in order to avoid internal circuit damage in the displays. Is there a way this can be ensured by programming the IMX6 processor to keep these line low or high impedance. Otherwise I need to provide an external buffers. I don't see this kind on design implementation on any Freescale boards.

ラベル(3)
0 件の賞賛
返信
3 返答(返信)

2,433件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Processor does not perform special actions for these display signals, that is at power up

they are inputs (100K impedance pull or keeper). Power up pads state one can find in Datasheet

section "Package Information and Contact Assignments".

0 件の賞賛
返信

2,433件の閲覧回数
rajniks
Contributor I

I understand that part of it. I was more looking into some control register setting for the Display IOs that does this job.

0 件の賞賛
返信

2,433件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Raj

if you are speaking about i.MX6, it has not speical Display module settings

for settings IOs low at power-up. One can set them later after power-up.

Best regards

chip

0 件の賞賛
返信