LVDS Display resolution

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LVDS Display resolution

Jump to solution
5,803 Views
pankajrana
Contributor III

What is the maximum resolution we can get by using only one LVDS Channel.?? As per information I think it is not possible to achieve 1080p HD resolution by using only one LVDS channel.

There is a 31.5 inch LVDS Display, having two channel input, and resolution 1920x1080. How is it possible to increase the resolution to get Full HD 1920x1080 ? i.e. what input must be supplied to the LCD input pins,?

Labels (6)
0 Kudos
Reply
1 Solution
4,756 Views
saurabh206
Senior Contributor III

Hi,

If you don't use split mode than you will not get the 1080P.

Dual Mode is used to display same data on two display.

You can try if you want, and share your result.

Thanks

Saurabh

View solution in original post

0 Kudos
Reply
6 Replies
4,756 Views
pankajrana
Contributor III

SergioSolis SaurabhPatel

Hello All,

Split mode is understood, but what if I don't go for SPLIT mode, instead I choose Dual Channel Mode.
i.e. Using only channel one , and then providing the same data to both the input ports of the Display.?

will that give a proper image/display, or will it spoil the contents !

Thanks.

Pankaj Rana

0 Kudos
Reply
4,757 Views
saurabh206
Senior Contributor III

Hi,

If you don't use split mode than you will not get the 1080P.

Dual Mode is used to display same data on two display.

You can try if you want, and share your result.

Thanks

Saurabh

0 Kudos
Reply
4,756 Views
saurabh206
Senior Contributor III

Hi,

To get 1080P you need to use two channel.

Saurabh

0 Kudos
Reply
4,756 Views
pankajrana
Contributor III

Hi Saurabh,

Using two channels is fine, even the Display supports that, but am worried about the mode to be used, Should I go with Dual Channel Mode , or Split Channel mode ?

Thanks.

Pankaj Rana

0 Kudos
Reply
4,756 Views
saurabh206
Senior Contributor III

Hi

You should use Split channel mode to get 1080P working...

Saurabh

4,756 Views
SergioSolis
NXP Employee
NXP Employee

Yes, you can achieve 1080p by using split channel mode.


Best regards,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------