LTP failed Imx8

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LTP failed Imx8

1,226件の閲覧回数
Haji1991
Contributor I

Hi, 

I am using IMX8 Board with 5.4 Linux Kernel.

When I am running the Linux Test Project(LTP) Test I'm getting Below failures in 

Test NoTest NameCommandFail Discription
1chdir01Asymlink01 -T chdir01chdir01 1 TFAIL : symlink01.c:1509: symlink(object, symbolic) was succesful.
mkdir(object, 0700) was successful
chdir(2) returned successfully, but getcwd(3) indicated new current working directory location /var/volatile/tmp/ltp-XXXXDZjggJ/chdyUIfjx/object not equal to expected /tmp/ltp-XXXXDZjggJ/chdyUIfjx/object
chdir01 2 TPASS : chdir(2) to non-existent object file location through symbolic link file failed as expected
chdir01 3 TPASS : Nested symbolic link access condition caught. ELOOP is returned
2msgstress03msgstress03msgstress03 1 TFAIL : msgstress03.c:155: Fork failed (may be OK if under stress)

 

Please suggest, what need to done for the above failures

 

Thanks & Regards,
Haji 

0 件の賞賛
返信
0 返答(返信)