LTIB resets my kernel config, while compiling

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LTIB resets my kernel config, while compiling

1,696件の閲覧回数
mmaaxx
Contributor III
Hello, I'm building a linux image for i.MX28, with LTIB, under Ubuntu 11.04 (also tried same under Ubuntu 9 on VMWare, by freescale). I noticed that some parameters of the kernel configuration that I selected from menuconfig or manually selected (by editing the config file) are not present in a kernel that I built. 

I did some debugging, and found that "scripts/kconfig/conf -o arch/arm/Kconfig" command right at the beginning of the build process resets some kernel settings.

Any way to fix this? 


Here is how it looks like:
Code:

+ cp -f /home/max/imx28/ltib/config/platform/imx/imx28evk_defconfig.dev ./.config
+ make ARCH=arm CROSS_COMPILE= HOSTCC=ccache /usr/bin/gcc -B/usr/bin/ oldconfig
+ yes
scripts/kconfig/conf -o arch/arm/Kconfig
#
# configuration written to .config
#

+ [ -f /home/max/imx28/ltib/config/platform/imx/imx28evk_defconfig.dev ]
+ diff -q ./.config /home/max/imx28/ltib/config/platform/imx/imx28evk_defconfig.dev
Files ./.config and /home/max/imx28/ltib/config/platform/imx/imx28evk_defconfig.dev differ
+ cp -f ./.config /home/max/imx28/ltib/config/platform/imx/imx28evk_defconfig.dev

 

Thanks!

ラベル(1)
1 返信

1,398件の閲覧回数
kirannevaskar
Contributor II

Hello Max Herman,

Thanks for your information.

I am facing same issue.

I want to try your solution. I am not sure where to do those changes.

Will you please provide me the the file where I need to apply your suggestions?

Thanks.

With Regards,

Kiran Nevaskar

0 件の賞賛
返信