Hi..
I'm working with iMX28 using LTIB environment.
I've a problem with u-boot-2009.08 when i make the boot from SD card.
The default speed was 50MHz and i've reduced it until 5MHz, but the problem remains.
Using SDHC verbatim there aren't problems under 25MHz of clock...with other sdhc cards the problem remains also using 5MHz.
There's also a list of command sent to the SDHC when it works in 4bits bus width.
I print the serial log...(I added some printf )
Thanks in advance!!
*********START BOOTLET power_prep******************
PowerPrep start initialize power...
Configured for 5v only power source. Battery powered oper ation disabled.
 Dec 1 201116:49:02
 FRAC 0x92925552
 memory type is DDR2
 Wait for ddr ready 1power 0x00820616
 Frac 0x92925552
 start change cpu freq
 hbus 0x00000003
 cpu 0x00010001
 start test memory accress
 ddr2 0x40000000
 finish simple test
 U-Boot 2009.08 (Dec 01 2011 - 12:11:56)
Freescale i.MX28 family
 CPU: 454 MHz
 BUS: 151 MHz
 EMI: 205 MHz
 GPMI: 24 MHz
 DRAM: 128 MB
 MMC: ***imx_ssp_mmc_initialize***
 ***imx_ssp_mmc_initialize***
 IMX_SSP_MMC: 0, IMX_SSP_MMC: 1
 MMC0: Set clock rate to 400 KHz (requested 400 KHz)
 ***ssp_mmc_init***
MMC0: Set 1 bits bus width
 MMC0: Set clock rate to 400 KHz (requested 400 KHz)
 MMC0: Set 1 bits bus width
 MMC0: CMD0
 MMC0: CMD8
 MMC0: CMD55
 MMC0: CMD41
 MMC0: CMD55
 MMC0: CMD41
 MMC0: CMD2
 MMC0: CMD3
 MMC0: CMD9
 MMC0: CMD7
 MMC0: CMD55
 MMC0: CMD51
 MMC0: CMD6
 MMC0: CMD6
 MMC0: CMD55
 MMC0: CMD6
 MMC0: Set clock rate to 400 KHz (requested 400 KHz)
 MMC0: Set 4 bits bus width
 u-boot-2009.08/driver/mmc/mmc.c *** mmc_set_clock: 20MHz ***
 MMC0: Set clock rate to 4965 KHz (requested 5000 KHz)
 MMC0: Set 4 bits bus width
 MMC0: CMD16
 MMC0: CMD17
 MMC0: CMD16
 MMC0: CMD18
 MMC0: CMD12
 *** Warning - bad CRC or MMC, using default environment
In: serial
 Out: serial
 Err: serial
 Net: got MAC address from IIM: 00:04:00:00:00:00
 FEC0
 Hit any key to stop autoboot: 3
Hi Nico,
First you have to change your environment variables from default.
Then the problem will be solved.
Link is here :: http://imxcommunity.org/group/imx53quickstartboard/forum/topics/user-experience-with-1109-binaries-w...
Try to figure out respective args for your i.MX from user manual.
Regards :: Krishna Pavan