LTIB library path

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LTIB library path

5,447 次查看
niklasmolin
Senior Contributor I

Hi.

If I want to add a pre-built package to my LTIB (including bin and lib), how do I add the lib path so the OS know where to look for that specific library?

Is there an environment variable where I include this lib-path?

In Ubuntu or debian I think they are using ld.so.conf, but I can't find that in LTIB.

Thanks,

Niklas

标记 (3)
0 项奖励
回复
11 回复数

4,618 次查看
Raybiztech
Contributor V

Hi Niklas,

                      The LTIB will look into "spec" files to build any particular package. so, if you want to build any package that uses your pre-built package. you need to export " bin, lib " paths, in that particular package spec file you need to build.

you can get the spec files at this location:

/ltib/dist/lfs-5.1/

-> In above path you can see spec file located in a directory with the name of package to be builded.

-> you can copy bin and lib folders into rootfs and export these paths in spec files.

These things i haven't tried u can use this as a reference.

Thanks & Regards,

Raybiztech.

0 项奖励
回复

4,618 次查看
niklasmolin
Senior Contributor I

Hi Raybiztech.

I finally had some time to start to look at this problem again (been busy with other parts).

If I compile some application in the ARM processor (not cross compiling) and I need to add library to the system, how do I do this in LTIB?

Thanks,

Niklas

0 项奖励
回复

4,618 次查看
LeonardoSandova
Specialist I

Are you tied to LTIB? I would suggest to also create a recipe for Yocto and bake it; you may find more documentation on this platform (yocto).

Leo

0 项奖励
回复

4,618 次查看
Raybiztech
Contributor V

To start using yocto look into this following thread

https://community.freescale.com/docs/DOC-94849

Thanks & Regards,

Raybiztech.

0 项奖励
回复

4,618 次查看
LeonardoSandova
Specialist I

Great, that is the best document as a starting point.

0 项奖励
回复

4,618 次查看
niklasmolin
Senior Contributor I

Hi.

One "quick" question.

How much memory do you think is necessary for running YOCTO?

I was first planning using 1GB, but now it looks like they are only going to give 512MB.

Would that be enough?

I'm not going to use any graphical interface.

Going run a web-server, plus backend code to handle interaction with HW etc.

Later one I'm going to include a database (not sure which yet, levelDB, couchDB etc.).

Regards,

Niklas

0 项奖励
回复

4,618 次查看
LeonardoSandova
Specialist I

RAM or HD? are you using a virtual machine? try to compile natively, the more RAM the better. For HD, you better have 100 GB so you do not run into trouble in the future. Yes, I wrote it right :smileyhappy:

Leo

0 项奖励
回复

4,617 次查看
niklasmolin
Senior Contributor I

Hi Leo.

I'm using a virtual machine for my compile.

I was more asking about the target (the Freescale where the YOCTO is going to run on).

On the sabrelite board there is 1GB RAM but it seems like I might only get 512MB on the final board.

I just wanted to check if it's enough?

Right now when I run the base image (with additional SDK etc.) I have around 850MB free. But now I'm not running any of my own applications yet.

/Niklas

0 项奖励
回复

4,618 次查看
LeonardoSandova
Specialist I

Niklas. Yocto does not run on the target, it run on host and  yields a system for the target. Not idea about the memory size but it your apps wont require much CPU/RAM, that may be enough.

Leo

0 项奖励
回复

4,617 次查看
Raybiztech
Contributor V

Hi Niklas,

                   If you want add any library to LTIB, you need to create a spec file for that particular library.

-> In  /ltib/dist/lfs-5.1/ create a directory on the name of the package you want to build

-> copy template.spec located in /ltib/dist/lfs-5.1/template/ directory to the new directory you had created to build your package.

-> cd to your package location for ex: /ltib/dist/lfs-5.1/sample/ rename template.spec to your package name. ex : sample.spec

-> open the sample.spec file and change modifications according to your requirement.

->save the spec file.

-> copy your package to /opt/frescale/pkgs/

-> cd to your LTIB path

-> ./ltib -m prep -p sample.spec (package name you added with .spec extension)

->./ltib -m scbuild -p sample.spec

->./ltib -m scinstall -p sample.spec

->./ltib -m scdeploy -p sample.spec

Thanks & Regards,

Raybiztech.

0 项奖励
回复

4,618 次查看
niklasmolin
Senior Contributor I

In Linux I assume we use ldconfig, is there a similar command in LTIB?

0 项奖励
回复