LTIB building error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LTIB building error

2,001 Views
andreyvarsegov
Contributor I

Hi all,

I want to make gst at my rootfs, but get error:

Processing: libfslcodec

=========================

Build path taken because: no prebuilt rpm,

Testing network connectivity

OK GPP:

Try libfslcodec-3.0.6.tar.gz.md5 from the GPP

http://bitshrine.org/gpp/libfslcodec-3.0.6.tar.gz.md5:

20:14:54 ERROR 404: Not Found.

Try libfslcodec-3.0.6.tar.gz from the GPP

http://bitshrine.org/gpp/libfslcodec-3.0.6.tar.gz:

20:14:55 ERROR 404: Not Found.

Can't get: libfslcodec-3.0.6.tar.gz at ./ltib line 802.

f_buildrpms() returned an error, exiting

traceback:

main:572

Where i can find libfslcodec-3.0.6.tar.gz.md5  and libfslcodec-3.0.6.tar.gz files?

Best regards, Andrey.

Labels (1)
0 Kudos
Reply
2 Replies

1,588 Views
Yuri
NXP Employee
NXP Employee
0 Kudos
Reply

1,588 Views
LeonardoSandova
Specialist I

Hi Andrey,

they are in a separate tarball on the freescale portal. Once you have them, untar the file under /var/tmp/pkgs (I am not 100% of the pathname but check the documentation please) and compile again (meaning, run ltib again)

Leo

0 Kudos
Reply