IMX6 Platform SDK update ??

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6 Platform SDK update ??

3,486件の閲覧回数
marktwainjr
Contributor II

Hello Freescale,

When can we expect update over Platform SDK v1.1 for IMX6?

we are more interested in USB host driver update specifically for Mass Storage devices.

Can anyone tell me which USB Host controller chip is used on IMX6q? is it same across kinetis boards?

Thanks,

MT

タグ(5)
0 件の賞賛
返信
5 返答(返信)

2,900件の閲覧回数
Yuri
NXP Employee
NXP Employee

As for i.MX6 USB - it uses ARC / Transdimension IP.

0 件の賞賛
返信

2,900件の閲覧回数
YixingKong
Senior Contributor IV

Yuri, could you continue the discussion with the customer?

Thanks,

Yixing

0 件の賞賛
返信

2,900件の閲覧回数
marktwainjr
Contributor II

Hello Yuri & All,

Thanks!!

What about USB IP in kinetis, is it same as used in IMX6?

How about using

USB Stack Product Summary Page

? Can we use this for imx6 psdk?

Q>>>>>When can we expect update over Platform SDK v1.1 for IMX6? Specifically updates for USB host driver update specifically for Mass Storage devices.

Thanks,

MT

0 件の賞賛
返信

2,899件の閲覧回数
YixingKong
Senior Contributor IV

Mark, please click Correct Answer/Helpful Answer if your questions have been answered.

Thanks,

Yixing

0 件の賞賛
返信

2,900件の閲覧回数
Yuri
NXP Employee
NXP Employee

I looked at "K20 Sub-Family Reference Manual". There are two USB modules here :

- Universal Serial Bus OTG Controller (USBOTG) ;

- USB High Speed OTG Controller (USBHS).

As I see, the USBHS is ARC IP based and it is very similar to i.MX6 OTG, at least,
so called USB-Core Registers. Note, the i.MX6 OTG also has so called non-core
(USB) registers, which are Freescale specific.
So, there is ARC USB core part of USB modules of i.MX6 and Kinetis which is practically
the same for both ones, but some specific registers also may be found.  
 

As for the USB Stack, the i.MX6 is not supported there (I think because of the mentioned specifics). 

0 件の賞賛
返信