Hello,
I'm trying to add openssh to my LTIB Linux build, but the build is failing because of Perl dependencies.
Here is the build error message:
.......
Processing files: openssl-1.0.1c-1
Finding Provides: (using /opt/freescale/ltib/usr/lib/rpm/find-provides)...
Finding Requires: (using /opt/freescale/ltib/usr/lib/rpm/find-requires)...
Provides: lib4758cca.so libaep.so libatalla.so libcapi.so libchil.so libcrypto.so.1.0.0 libcswift.so libgmp.so libgost.so libnuron.so libpadlock.so libssl.so.1.0.0 libsureware.so libubsec.so
PreReq: rpmlib(PayloadFilesHavePrefix) <= 4.0-1 rpmlib(CompressedFileNames) <= 3.0.4-1
Requires(rpmlib): rpmlib(PayloadFilesHavePrefix) <= 4.0-1 rpmlib(CompressedFileNames) <= 3.0.4-1
Requires: /bin/sh /usr/bin/perl libc.so.6(GLIBC_2.4) libc.so.6(GLIBC_2.7) libdl.so.2(GLIBC_2.4) libgcc_s.so.1(GCC_3.5) perl(File::Basename) perl(Getopt::Std) perl(IO::Handle) perl(WWW::Curl::Easy) perl(strict) perl(vars)
Wrote: /opt/ltib_imx6/ltib/rpm/RPMS/arm/openssl-1.0.1c-1.arm.rpm
Executing(%clean): /bin/sh -e /opt/ltib_imx6/ltib/tmp/rpm-tmp.80224
+ umask 022
+ cd /opt/ltib_imx6/ltib/rpm/BUILD
+ cd openssl-1.0.1c
+ rm -rf /opt/ltib_imx6/ltib/tmp/openssl
+ exit 0
Executing(--clean): /bin/sh -e /opt/ltib_imx6/ltib/tmp/rpm-tmp.80224
+ umask 022
+ cd /opt/ltib_imx6/ltib/rpm/BUILD
+ rm -rf openssl-1.0.1c
+ exit 0
Build time for openssl: 95 seconds
sudo /opt/freescale/ltib/usr/bin/rpm --root /opt/ltib_imx6/ltib/rootfs --dbpath /var/lib/rpm -e --allmatches --nodeps --define '_tmppath /tmp/ltib' openssl 2>/dev/null
sudo /opt/freescale/ltib/usr/bin/rpm --root /opt/ltib_imx6/ltib/rootfs --dbpath /var/lib/rpm --prefix / --ignorearch -ivh --force --excludedocs --define '_tmppath /tmp/ltib' /opt/ltib_imx6/ltib/rpm/RPMS/arm/openssl-1.0.1c-1.arm.rpm
error: failed dependencies:
perl(IO::Handle) is needed by openssl-1.0.1c-1
perl(WWW::Curl::Easy) is needed by openssl-1.0.1c-1
f_buildrpms() returned an error, exiting
traceback:
main:572
Started: Fri Jun 13 10:57:07 2014
Ended: Fri Jun 13 11:05:20 2014
Elapsed: 493 seconds
Build Failed
Exiting on error or interrupt
---------------------------------------------------------------------------------------------------------------------------------------------------------------
What libraries/modules am I missing?
I've tried adding perl-5.8.8.tar.gz in /opt/freescale/pkgs as well as enabled perl in the config screen, but it hasn't helped.
Here's my setup:
- Reference board used: Sabre SD board - MCIMX6Q SDB
- Kernel version: LTIB Linux 3.0.35
Thanks,
Mithun
 
					
				
		
 jamesbone
		
			jamesbone
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		gusarambula, Check this is out!
Sorry, was there an attachment or a link?
 
					
				
		
 gusarambula
		
			gusarambula
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		The LTIB host setup depends a lot on the Ubuntu distribution you’re using. As you might have noticed Ubuntu 9.04 is the recommended version although it’s a bit outdated.
Some of the users in the community have been able to install LTIB successfully on Ubuntu 12.04 and 13.04 with some tweaks. Which version are you using?
In case you are using Ubuntu 12.04 please install the patch found on the following document:
https://community.freescale.com/docs/DOC-93455
In case you are using Ubuntu 13.04 install this patch and perform the tweaks on the answer to the following thread:
I am having this issue on 10.04.
I've no idea why, but if I execute
./ltib -m prep -p openssl
./ltib
Then it succeeds. But if I don't prep the package first, something fails afterward. For example:
rm -rf rpm/BUILD/openssl*
rm -rf rpm/RPMS/arm/openssl*
./ltib
I noticed that even when it fails with all those perl dependencies, the rpm has already been built. It's breaking during the installation I think, when it tries to compute the "find-requires". Somehow, having the source tree around causes the find-requires part to pass for me.
Anyway, perhaps this is why people are having trouble reproducing this and saying "it works for me". Probably anyone trying to solve this problem would prep the package and work on the openssl source, masking the problem.
If anyone can explain what's really going on here, please do tell.
I forgot to mention:
I'm using Ubuntu 9.04 and I am able to successfully build the kernel if I don't include openssh.
It's only when I add openssh that I run into problems.
Are there any patches for 9.04?
 
					
				
		
 jamesbone
		
			jamesbone
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello M.G.
Do you think you can share the configuration that you use in your LTIB, you can review in the details of the package the depencys that need to be selected in order to get the SSH to compile. I think you are missing a package in order to get the kernel build.
Have a great day,
Jaime
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I'm not sure which configuration files you would like to see, but I have attached 2 which I could find relevant.
I've renamed them as .config1 and .config2.
.config1 -> /opt/ltib_imx6/ltib/rpm/BUILD/linux-3.0.35/.config
.config2 -> /opt/ltib_imx6/ltib/config/platform/imx/.config
Let me know if you were looking for some other files, and where I can find them.