LTIB Config

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LTIB Config

2,639件の閲覧回数
曦刘
Contributor II

I used "L3.0.35_4.1.0_130816_source.tar.gz" make ltib -m config in Ubuntu 10.04  version

there are some error in the host_config.log file:

Processing platform: Host support packages

============================================

using /home/L3.0.35_4.1.0_130816_source/ltib/config/platform/host/ltib.preconfig

Processing: fake-provides

===========================

Processing: mkspooflinks

==========================

Processing: distcc

====================

Processing: ccache

====================

Processing: m4

================

Processing: bison

===================

Processing: flex

==================

Build path taken because: directory build, no prebuilt rpm,

Cowardly refusing to clobber existing directory:

/opt/freescale/ltib/usr/src/rpm/BUILD/flex-2.5.37

Remove this by hand if you really want to rebuild this package from scratch

Died at ./ltib line 1392.

traceback:

main::build_host_rpms:1392

  main::host_checks:1447

   main:554

ラベル(2)
3 返答(返信)

2,034件の閲覧回数
LeonardoSandova
Specialist I

have you done what the log suggest (removing that folder)?

Leo

0 件の賞賛
返信

2,034件の閲覧回数
曦刘
Contributor II

it can config now,

after i delet the "/opt/frescale"

and install texinfo texlive.

Thaks

2,034件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

To install and build LTIB, the first step is to remove all previously-installed packages in /opt/freescale/pkgs/. As we can see it in every board User Guide.

Best Regards

Dan