Hi all,
I'm working on a i.MX95 board, and I'm running into issues enabling LPUART2 from Linux.
I've added the following to my board-specific .dts:
&lpuart2 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_uart2>;
status = "okay";
};
(this much should work as other uart working with similar changes)
The pinctrl is properly defined and the DT compiles correctly. However, during kernel boot, I get this error:
scmi-pinctrl scmi_dev.6: Error parsing config -13
scmi-pinctrl scmi_dev.6: pin_config_set op failed for pin 119
fsl-lpuart 44390000.serial: Error applying setting, reverse things back
Internal error: synchronous external abort: 0000000096000010 [#1] PREEMPT SMP
If I disable LPUART2, the kernel boots normally.
So I'm wondering if something in the system or firmware is preventing access to this UART from the Linux side.
Appreciate any insights, thanks!
Let me know if you'd like me to share the full DTS file or any kernel logs again.
>> Your board are using the UART2 for M core?
I'm not entirely certain how the core ownership is configured on this platform, but based on the imx95-iwg61m.dtsi file, UART2 is commented as // M33 UART , which suggests that it may be allocated to the M core (Cortex-M33).
If that’s the case, I assume the UART2 peripheral might be under the control of the M core, and that could explain the issue when the A core tries to configure or access it.
Could you please confirm if UART2 is reserved for the M core by default in this SoC? If so, I’d like to understand the proper method to reassign or release it for use by the A core. Is it done via SCMI resource partitioning or any specific firmware configuration?
For reference, during kernel boot, I'm getting the following error:
i have already shared the error snippet while kernel is starting that
scmi-pinctrl scmi_dev.6: Error parsing config -13
scmi-pinctrl scmi_dev.6: pin_config_set op failed for pin 119
fsl-lpuart 44390000.serial: Error applying setting, reverse things back
Internal error: synchronous external abort: 0000000096000010 [#1] PREEMPT SMP
This seems to point toward either access permission issues or improper ownership configuration.
>>What boards are you using?
I am using iwave i.MX 95 SMARC SOM
Hi @Samt07!
The iMX95 could contain embedded the binary of M core in the boot loader image..
I recommend to ask to iWAVE how to remove the image of the M core of their image to use the UART2 in A core.
Both processors can´t use the same peripheral because can cause kernel panics.
Is a normal behavior and that happens in iMX8M too when the peripherals are taken by two different cores.
Best Regards!
Chavira