LPSPI multibyte transfer without CS toggle

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPSPI multibyte transfer without CS toggle

5,577 Views
hansung_jung
Contributor III

Hello,

I use FRAM (Fujitsu, mb85rs1mt) on an I.MX8qxp processor. I run SCLK, MISO, MOSI, CS for SPI connections. But CS doesn't work the way I expect it to.

FRAM is based on fujitsu, mb85rs1mt drivers and operates in compatible mode with jedec, spi-nor drivers.

To read the ID of the FRAM, you must send command bytes and read three more data bytes. The CS must remain low throughout the entire sequence.

However, since CS rises per byte, the ID of FRAM cannot be read because the rising edge interferes with communication.

I found and applied on Google that if I set the CS pin as regular GPIO, I can read the ID of FRAM, but in this case, I can't control the CS pin at all.

The kernel version is 5.10.35, and a custom board is being created and implemented.

0 Kudos
Reply
13 Replies

5,423 Views
pengyong_zhang
NXP Employee
NXP Employee
0 Kudos
Reply

5,440 Views
pengyong_zhang
NXP Employee
NXP Employee

Hi, @hansung_jung 

The config file is empty. Do not need to modify the config file.

Please share your board HW schematic diagram, Have you checked whether the GPIO has been occupied?

B.R

0 Kudos
Reply

5,428 Views
hansung_jung
Contributor III

I am sorry that the attached config file had hide property.

Anyway, I understood it does not matter.

Please refer below schematic diagram.

hansung_jung_1-1704954184366.png

And I checked all gpio but the SPI1_CS0 pin is assigned only for cs.

I think it is very interesting that it works at your board.

I have to search more.

Thanks for your support.

 

 

0 Kudos
Reply

5,455 Views
pengyong_zhang
NXP Employee
NXP Employee

Hi, @hansung_jung 

Please refer below code, add the "cs-gpios = <&lsio_gpio1 8 GPIO_ACTIVE_LOW>;" to your dts file.

&lpspi0 {
    fsl,spi-num-chipselects = <1>;
    pinctrl-names = "default";
    pinctrl-0 = <&pinctrl_lpspi0 &pinctrl_lpspi0_cs>;
    cs-gpios = <&lsio_gpio1 8 GPIO_ACTIVE_LOW>;
    status = "okay";
 
};
I have tested today, cs signal voltage change is no problem. During the data transmission process, it continues to maintain a low level until the data transmission is completed and returns to a high level.
 
B.R
0 Kudos
Reply

5,453 Views
hansung_jung
Contributor III

Thanks for your support, but unfortunetly CS pin does not work.

Refer below scope wave, and my dts file.

hansung_jung_2-1704882448623.png

hansung_jung_1-1704882344822.png

hansung_jung_0-1704882305769.png

Is there anything else I need to check, like .config?

Could you look at my .config just in case?

Please refer the attached file.

0 Kudos
Reply

5,472 Views
pengyong_zhang
NXP Employee
NXP Employee

Hi, @hansung_jung 

Pleae use the following setting to test:

    pinctrl_lpspi0: lpspi0grp {
        fsl,pins = <
            IMX8QXP_SPI0_SCK_ADMA_SPI0_SCK      0x6000040
            IMX8QXP_SPI0_SDO_ADMA_SPI0_SDO      0x6000040
            IMX8QXP_SPI0_SDI_ADMA_SPI0_SDI      0x6000040
        >;
    };

    pinctrl_lpspi0_cs: lpspi0cs {
        fsl,pins = <
            IMX8QXP_SPI0_CS0_LSIO_GPIO1_IO08    0x21
        >;
    };
 
    pinctrl-0 = <&pinctrl_lpspi0 &pinctrl_lpspi0_cs>;
 
B.R
 
0 Kudos
Reply

5,470 Views
hansung_jung
Contributor III

Thanks for your solution, however CS does not work.

I attach oscilloscope wave image.

hansung_jung_0-1704865516371.png

And this is my dts modified as you suggested.

hansung_jung_1-1704865596736.png

hansung_jung_2-1704865645832.png

0 Kudos
Reply

5,512 Views
pengyong_zhang
NXP Employee
NXP Employee

Hi, @hansung_jung 

It looks like your settings are correct. I will try to reproduce your problem.

Which dts file are you using? Have you tried using other GPIO as CS?

B.R

0 Kudos
Reply

5,510 Views
hansung_jung
Contributor III

Yes, I tried to use other gpio as cs, however it was same result.

Please refer below.

hansung_jung_0-1704793320670.png

 

0 Kudos
Reply

5,544 Views
pengyong_zhang
NXP Employee
NXP Employee

Hi, @hansung_jung 

Please share your dts file.

B.R

0 Kudos
Reply

5,539 Views
hansung_jung
Contributor III

Thanks for your rapid reply.

I attached my dts file.

imx8qxp_dts.jpg

0 Kudos
Reply

5,554 Views
pengyong_zhang
NXP Employee
NXP Employee

Hi, @hansung_jung 

when you set the CS pin as regular GPIO.What do you  mean you can't control the CS pin at all? Do you want to control CS level variation during spi communication?

B.R

0 Kudos
Reply

5,546 Views
hansung_jung
Contributor III

Looking at the link below, I thought it would be okay to change cs from native control to gpio control.
However, it was confirmed that there was no change at all when the waveform was measured with the cs pin with the oscilloscope when it was changed to gpio control.

Solved: SPI - F-RAM usage on Linux - NXP Community

0 Kudos
Reply