LPSPI driver is not able to work with external flash on imrt1051CVL5B target board.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPSPI driver is not able to work with external flash on imrt1051CVL5B target board.

773 Views
venkataddagatla
Contributor II

We are working on verifying the memory interfaces by using LPSPI3 on the imxrt1051 microcontroller.

We are using the LPSPI driver to communicate the flash and fram.

There are 3 memory interfaces connected on LPSPI3 (2 flash and FRAM).

We generated the LPSI driver from the configuration tool and We are able to read the vendor id/ Manufacturer id of all the Memory chips(MX25L6433F, FM25V02).

But we could not able to get the white enable status set even after send Write enable command to flash.

 

 

Labels (1)
0 Kudos
Reply
1 Reply

764 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Did you ever check the SPI signal by using the logic analyzer or oscilloscope? If not, please give it a try and share the captured signal with me, as it can provide some clues.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply