LPDDRAM bringup instruction

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPDDRAM bringup instruction

Jump to solution
1,778 Views
khang_letruong
Senior Contributor III

Dear Community,

I'm about bringing up a custom iMX8MP based SoM using BD71847AMWV-E2 PMIC and Micron MT53E256M32D2DS-053 LPDDR4. I would be very thankful if someone could provide me instruction / steps to configure the previously-mentioned memory for the bring-up. Especially what are the key parameters the could be found from its datasheet/specification, please ?

I find following link good starting point : https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/110...

I also found this link for iMX8M Mini : https://community.nxp.com/t5/i-MX-Processors/NXP-DDR-Tool-v3-10-i-MX8MMini-Please-re-download-with-t...

Thanks in advance and best regards,
Khang.

0 Kudos
Reply
1 Solution
1,770 Views
Yuri
NXP Employee
NXP Employee
0 Kudos
Reply
1 Reply
1,771 Views
Yuri
NXP Employee
NXP Employee
0 Kudos
Reply