Hi NXP,
Do you have any processor that can support LPDDR4 device with 4 channels (64-bit)?
This 4 channel LPDDR4 device only has 1 RESET_n pin.
Can I use two iMX8MP processors to support this device? The 1st iMX8MP connects to channel A and channel B. The 2nd iMX8MP connects to channel C and channel D. The RESET_n pin connects to either one of the iMX8MP. Is it possible?
Please help.
Hi Simon
>Do you have any processor that can support LPDDR4 device with 4 channels
if this is two die device seems it is possible with i.MX8M Plus, as it have CS0,CS1 lines
as depicted below (from SPF-46368 p.5 i.MX8M Plus EVK schematic)
>Can I use two iMX8MP processors to support this device?
no
Best regards
igor
seems such parts can not be supported by i.MX8M Plus, sorry.
Best regards
igor