LPDDR4 with 4 channels (64-bit)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPDDR4 with 4 channels (64-bit)

863件の閲覧回数
simonng
Contributor III

Hi NXP,

Do you have any processor that can support LPDDR4 device with 4 channels (64-bit)?

This 4 channel LPDDR4 device only has 1 RESET_n pin.

Can I use two iMX8MP processors to support this device? The 1st iMX8MP connects to channel A and channel B. The 2nd iMX8MP connects to channel C and channel D. The RESET_n pin connects to either one of the iMX8MP. Is it possible?

Please help.

0 件の賞賛
返信
4 返答(返信)

860件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Simon

 

>Do you have any processor that can support LPDDR4 device with 4 channels

 

if this is two die device seems it is possible with i.MX8M Plus, as it have CS0,CS1 lines

as depicted below (from SPF-46368 p.5 i.MX8M Plus EVK schematic)

 

1.jpg

 

>Can I use two iMX8MP processors to support this device?

 

no

 

Best regards
igor

0 件の賞賛
返信

857件の閲覧回数
simonng
Contributor III

Hi igor,

I think only two CS is not enough. Please check the block diagram below.

simonng_0-1641362423254.png

 

0 件の賞賛
返信

852件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

seems such parts can not be supported by i.MX8M Plus, sorry.

 

Best regards
igor

0 件の賞賛
返信

846件の閲覧回数
simonng
Contributor III

Hi igor,

Is there any NXP processor that can support this 4 channel LPDDR4 device?

Regards,

Simon

0 件の賞賛
返信