LPDDR4 tracing for imx8mini

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPDDR4 tracing for imx8mini

1,120件の閲覧回数
vladimirsirik
Contributor I

one of my ctm has the question related to LPDDR4 tracing for imx8mini - 

there is the Table 31. "i.MX 8M Mini DDR package trace delays" into the « i.MX 8M Mini Hardware Developer’s Guide» with the delays into the picoseconds.

Question - to match LPDDR4 lines (for delays) we need to convert the PCB line lengths  into the delays. Please advise which formula we should use for it? For the waves propagating into the dielectric or into the air?  

Thanks for your help.

ラベル(1)
0 件の賞賛
返信
1 返信

1,055件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

  Recommendation is as following: to calculate the package trace lengths from the

package delays customers can use the rule of thumb - 6mils/ps.

   

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 件の賞賛
返信