LPDDR4 capacity for MIMX8QM6AVUFFAB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPDDR4 capacity for MIMX8QM6AVUFFAB

2,480 Views
tw_wang
Contributor I

Could we change the  LPDDR4 capacity from 6GB to the 4GB or 8GB on the MIMX8QM6AVUFFAB referece design ?

0 Kudos
Reply
4 Replies

2,451 Views
Mestkim
Contributor III

i.MX 8/8X Family DDR Tools Release - NXP Community

 

3. Change 0x980000000 to 0xA00000000 in the above chunk of code. That should allow for 8GB density for MX8QM example shown above (for MX8QXP, change 0x8C0000000ULL to 0x900000000ULL for 4GB density).

0 Kudos
Reply

2,463 Views
joanxie
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

2,449 Views
Mestkim
Contributor III

i.MX8QM MEK board is 6GB. 

tw wang knows the i.MX8QM MEK is 6GB.

But you don't know.

and you don't know what is per controller in i.MX 8/8X/8XLite - LPDDR4 and DDR3L memory compat... - NXP Community 

 

0 Kudos
Reply

2,428 Views
joanxie
NXP TechSupport
NXP TechSupport

yes, the imx8qm supports 4GB(per controller) max, this is my misunderstanding, I thought tw_wang needs 8GB/controller, for total 8GB, this is patch

SCFW lilmits the DDR size to 6GB both in DDR tool and Linux BSP.

1. Replace mx8qmb0_scfw_download.bin in DDR_tool/bin with the attached binary. You can stress test all 8GB memory size with your DDR script.

2. Modify board_system_config() in board.c in your SCFW project as follows

/* Board has 6GB8GB memory so fragment upper region and retain 4GB */

        BRD_ERR(rm_memreg_frag(pt_boot, &mr_temp, 0x980000000ULL, 0xA00000000ULL,

            0xFFFFFFFFFULL));

0 Kudos
Reply