LPDDR4 Impedance Configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPDDR4 Impedance Configuration

2,869 Views
FanS2023
Contributor I

Hello:

 

imx8mp基板经过仿真后,需要配置驱动阻抗60Ω,ODT为40Ω

用工具‘MX8M_Plus_LPDDR4_RPA_v8’进行配置

请求帮忙确认,配置方法是否正确,配置内容如下:

242.jpg

 

250.jpg

 

468.jpg

 

476.jpg

 

599.jpg

 

607.jpg

638.jpg

644.jpg

651.jpg

657.jpg

664.jpg

670.jpg

673.jpg

十分感谢!   

0 Kudos
Reply
4 Replies

2,830 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

可以的,如果你的DDR测试有问题的话,我们可以帮忙reviewMX8M_Plus_LPDDR4_RPA,这里建议你用最新的版本https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8MPlus-m865S-DDR-Register-Programmi...

2,815 Views
FanS2023
Contributor I

再请教下

 

软件仿真最优时Driver 60ohm、ODT40ohm,

基板设计的线路单端阻抗时50±10%(45-55)ohm,

这样是否对传输信号的质量有影响?

 

以上

0 Kudos
Reply

2,798 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

所有单端信号为50欧姆阻抗,误差+/-10%,无论是怎么模拟,都是这个规则。

PCB制板过程中,影响到阻抗的因素很多,1. 板材材料偏差,2 PCB蚀刻时的偏差,加工过程中产生的偏差,3, 高速PCB时,甚至连铜箔的光洁度都对阻抗有影响。

40欧姆,60欧姆,。。。看上去似乎很精确,但是模拟过程中,没有实际制板过程的因素。

0 Kudos
Reply

2,822 Views
FanS2023
Contributor I

好的,谢谢你!

已经测试,没有问题

0 Kudos
Reply