LPDDR3 parameter selection for i.MX6ULL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPDDR3 parameter selection for i.MX6ULL

跳至解决方案
2,623 次查看
ko-hey
Senior Contributor II

Hi all

 

I have a question about I.MX6ULL DDR3 Script Aid which is download from below.

https://community.nxp.com/docs/DOC-333791

 

My customer choose MT41K256M16TW-107 IT:P due to the device availability.

 

 

Q1.

I know that i.MX6ULL only support 800MB/s.

When the speed grade of DDR3L connected to IMX 6ULL is DDR 3-1866, can we select DDR3-1866 in "Memory Type” field of the Register configuration sheet ?

 

 

Q2.

In above case, can we follow the parameter of speed grade for 107 ?

 

 

Ko-hey

 

标签 (4)
0 项奖励
回复
1 解答
2,113 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

1. customer can sellect 1600 grade for 1866 grade design (seems

DDR3-1600  option is max. in DDR3 Script Aid)

2. should be followed 1600 parameters and Table 1 footnote1 states:

107- Backward compatible to 1600.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,114 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

1. customer can sellect 1600 grade for 1866 grade design (seems

DDR3-1600  option is max. in DDR3 Script Aid)

2. should be followed 1600 parameters and Table 1 footnote1 states:

107- Backward compatible to 1600.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复