LPDDR initial check for custom board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPDDR initial check for custom board

Jump to solution
851 Views
Robbi
Contributor II

Hi Team, 

                 we had designed a custom-board with imx-93 processor. As a part of board bring-up activity. Need to test LPDDR4 ,eMMC and other peripherals. Is there any approach to test in u-boot stage with flashing image.

 

 

Thanks,,

Robbi.

0 Kudos
Reply
1 Solution
826 Views
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

For testing DDR, you would need to use Config Tools for the i.MX 93, you have to port your timings and characteristics into a new imx-boot image, the bring up is done through this interface and the test would be to get to U-boot after each boot.

For other interfaces like eMMC and so on, upon successfully porting your new imx-boot image with a custom u-boot, you could test your own code in the board.c file and/or through the U-boot commands, e.g. mmc read/ mmc write.

Regards

View solution in original post

0 Kudos
Reply
2 Replies
827 Views
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

For testing DDR, you would need to use Config Tools for the i.MX 93, you have to port your timings and characteristics into a new imx-boot image, the bring up is done through this interface and the test would be to get to U-boot after each boot.

For other interfaces like eMMC and so on, upon successfully porting your new imx-boot image with a custom u-boot, you could test your own code in the board.c file and/or through the U-boot commands, e.g. mmc read/ mmc write.

Regards

0 Kudos
Reply
793 Views
Robbi
Contributor II

Thanks @JosephAtNXP , Is there any sample application to test eMMC and QSPI NOR FLASH memory(instead of using mmc or dd commands).

 

 

0 Kudos
Reply