LOCSC X CSI CMOS Sensor Interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LOCSC X CSI CMOS Sensor Interface

ソリューションへジャンプ
3,439件の閲覧回数
rubensjunior
Contributor IV

Dear Collegues,

kerryzhou‌

igorpadykov‌

jeremyzhou‌

fangfang‌

jorgeantonioalcala‌

The LOCSC is a CMOS interface (No NXP).

I need to migrate a project that uses a LOCSC to CMOS Sensor Interface (CIS) using the iMXRT1051 processor. How I do?

Best Regards,

Rubens Júnior

ラベル(1)
1 解決策
3,262件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Rubens Junior,

Thanks for your reply.
1) Do you have something about this?
-- Unfortunately, we don't have some application notes or guides for this.

Have a great day,

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

4 返答(返信)
3,262件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Rubens Junior,

Thank you for your interest in NXP Semiconductor products and
the opportunity to serve you.
Actually, I'm not very clear about your mean, whether you want a guide or an application note which demonstrates how to use the CSI module to work with the CMOS sensor which supports the LOCSC protocol.

Have a great day,

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

3,262件の閲覧回数
rubensjunior
Contributor IV

Hi jeremyzhou‌,

Thank you very much!

You understanded correctly. I need to " a guide or an application note which demonstrates how to use the CSI module to work with the CMOS sensor which supports the LOCSC protocol".

Do you have something about this?

Best regards.

Rubens Júnior

0 件の賞賛
返信
3,263件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Rubens Junior,

Thanks for your reply.
1) Do you have something about this?
-- Unfortunately, we don't have some application notes or guides for this.

Have a great day,

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

3,262件の閲覧回数
rubensjunior
Contributor IV

Ok jeremyzhou‌! Thanks for your reply.

0 件の賞賛
返信