LINE_OUT and MIC_IN not working simultaneously in andorid 15

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LINE_OUT and MIC_IN not working simultaneously in andorid 15

519 次查看
subash_p
Contributor III

Hi,

I am using an i.MX8MP custom board with the SGTL5000 audio chip. Using TinyPlay, I can able to record and play WAV files from the Android 15 console. However, in the UI, I cannot use the microphone and speaker simultaneously. If I set the device speaker to SGTL5000, the recorder app cannot record (mic_in not detected). But if I disable the device speaker, I can able to record sound using the recorder app.


I will attach my DTS nodes and configuration files below.

sound {
compatible = "fsl,sgtl5000";
model = "sgtl5000";
codec-master;
ssi-controller = <&sai3>;
audio-codec = <&codec>;
audio-routing = 
    "MIC_IN", "Mic Jack",
            "Mic Jack", "Mic Bias",
            "Headphone Jack", "HP_OUT",
            "LINE_IN", "Line In Jack",
            "Line Out Jack", "LINE_OUT";
no-audmux;
};

 
codec: sgtl5000@a {
compatible = "fsl,sgtl5000";
reg = <0x0a>;
clocks = <&audio_blk_ctrl IMX8MP_CLK_AUDIOMIX_SAI3_MCLK1>;
clock-names = "mclk";
pinctrl-names = "default";
};

<-----------audio_policy_configuration.xml---------------->

<?xml version="1.0" encoding="UTF-8" standalone="yes"?>
<!-- Copyright (C) 2017 The Android Open Source Project

Licensed under the Apache License, Version 2.0 (the "License");
you may not use this file except in compliance with the License.
You may obtain a copy of the License at

http://www.apache.org/licenses/LICENSE-2.0

Unless required by applicable law or agreed to in writing, software
distributed under the License is distributed on an "AS IS" BASIS,
WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
See the License for the specific language governing permissions and
limitations under the License.
-->

<audioPolicyConfiguration version="7.0" xmlns:xi="http://www.w3.org/2001/XInclude">
<globalConfiguration speaker_drc_enabled="true"/>

<modules>
<module name="primary" halVersion="2.0">
<attachedDevices>
<item>Speaker</item>
<item>Built-In Mic</item>
</attachedDevices>
<defaultOutputDevice>Speaker</defaultOutputDevice>
<mixPorts>
<mixPort name="primary output" role="source" flags="AUDIO_OUTPUT_FLAG_PRIMARY">
<profile name="" format="AUDIO_FORMAT_PCM_16_BIT"
samplingRates="48000" channelMasks="AUDIO_CHANNEL_OUT_STEREO"/>
</mixPort>
<mixPort name="lpa output" role="source" flags="AUDIO_OUTPUT_FLAG_DIRECT AUDIO_OUTPUT_FLAG_HW_AV_SYNC">
<profile name="" format="AUDIO_FORMAT_PCM_16_BIT"
samplingRates="48000" channelMasks="AUDIO_CHANNEL_OUT_STEREO"/>
</mixPort>
<mixPort name="hdmi output" role="source">
<profile name="" format="AUDIO_FORMAT_PCM_8_24_BIT"
samplingRates="48000" channelMasks="AUDIO_CHANNEL_OUT_STEREO"/>
</mixPort>
<mixPort name="bt sco output" role="source">
<profile name="" format="AUDIO_FORMAT_PCM_16_BIT"
samplingRates="16000" channelMasks="AUDIO_CHANNEL_OUT_STEREO"/>
</mixPort>
<mixPort name="passthrough output" role="source" flags="AUDIO_OUTPUT_FLAG_DIRECT">
<profile name="" format="AUDIO_FORMAT_PCM_16_BIT"
samplingRates="48000 192000" channelMasks="AUDIO_CHANNEL_OUT_STEREO"/>
</mixPort>
<mixPort name="compressed_offload" role="source"
flags="AUDIO_OUTPUT_FLAG_DIRECT AUDIO_OUTPUT_FLAG_COMPRESS_OFFLOAD">
<profile name="" format="AUDIO_FORMAT_MP3"
samplingRates="8000 11025 12000 16000 22050 24000 32000 44100 48000"
channelMasks="AUDIO_CHANNEL_OUT_STEREO AUDIO_CHANNEL_OUT_MONO"/>
</mixPort>

<mixPort name="primary input" role="sink">
<profile name="" format="AUDIO_FORMAT_PCM_16_BIT"
samplingRates="8000 11025 16000 22050 32000 44100 48000"
channelMasks="AUDIO_CHANNEL_IN_MONO AUDIO_CHANNEL_IN_STEREO"/>
</mixPort>
<mixPort name="bt sco input" role="sink">
<profile name="" format="AUDIO_FORMAT_PCM_16_BIT"
samplingRates="16000" channelMasks="AUDIO_CHANNEL_IN_STEREO"/>
</mixPort>
</mixPorts>
<devicePorts>
<devicePort tagName="Speaker" type="AUDIO_DEVICE_OUT_SPEAKER" role="sink" >
</devicePort>
<devicePort tagName="Wired Headphones" type="AUDIO_DEVICE_OUT_WIRED_HEADPHONE" role="sink">
</devicePort>
<devicePort tagName="Wired Headset" type="AUDIO_DEVICE_OUT_WIRED_HEADSET" role="sink">
</devicePort>
<devicePort tagName="Line-Out" type="AUDIO_DEVICE_OUT_LINE" role="sink">
</devicePort>
<devicePort tagName="HDMI Out" type="AUDIO_DEVICE_OUT_AUX_DIGITAL" role="sink">
</devicePort>
<devicePort tagName="BT SCO Headset" type="AUDIO_DEVICE_OUT_BLUETOOTH_SCO_HEADSET" role="sink">
</devicePort>
<devicePort tagName="BT SCO CarKit" type="AUDIO_DEVICE_OUT_BLUETOOTH_SCO_CARKIT" role="sink">
</devicePort>
<devicePort tagName="BT SCO" type="AUDIO_DEVICE_OUT_BLUETOOTH_SCO" role="sink">
</devicePort>
<devicePort tagName="Built-In Mic" type="AUDIO_DEVICE_IN_BUILTIN_MIC" role="source">
</devicePort>
<devicePort tagName="Wired Headset Mic" type="AUDIO_DEVICE_IN_WIRED_HEADSET" role="source">
</devicePort>
<devicePort tagName="BT SCO Headset Mic" type="AUDIO_DEVICE_IN_BLUETOOTH_SCO_HEADSET" role="source">
</devicePort>
</devicePorts>
<routes>
<route type="mix" sink="Speaker"
sources="primary output"/>
<route type="mix" sink="Wired Headphones"
sources="primary output"/>
<route type="mix" sink="Wired Headset"
sources="primary output"/>
<route type="mix" sink="Line-Out"
sources="compressed_offload,lpa output,primary output"/>
<route type="mix" sink="HDMI Out"
sources="passthrough output,hdmi output"/>
<route type="mix" sink="BT SCO Headset"
sources="bt sco output"/>
<route type="mix" sink="BT SCO CarKit"
sources="bt sco output"/>
<route type="mix" sink="BT SCO"
sources="bt sco output"/>

<route type="mix" sink="primary input"
sources="Wired Headset Mic,Built-In Mic"/>
<route type="mix" sink="bt sco input"
sources="BT SCO Headset Mic"/>
</routes>
</module>

<!-- A2dp Input Audio HAL -->
<xi:include href="a2dp_in_audio_policy_configuration_7_0.xml"/>

<!-- Usb Audio HAL -->
<xi:include href="usb_audio_policy_configuration.xml"/>

<!-- Remote Submix Audio HAL -->
<xi:include href="r_submix_audio_policy_configuration.xml"/>

<!-- Bluetooth Audio HAL -->
<xi:include href="bluetooth_audio_policy_configuration_7_0.xml"/>

</modules>

<!-- Volume section -->
<xi:include href="audio_policy_volumes.xml"/>
<xi:include href="default_volume_tables.xml"/>

</audioPolicyConfiguration>




Thanks & regards,
Subash P.

标记 (4)
0 项奖励
回复
4 回复数

379 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Do you have the 8MP EVK board if the same happens on 8MP EVK board?

@subash_p 

0 项奖励
回复

326 次查看
subash_p
Contributor III

Hi @Rita_Wang 

No, EVK board is not with me.


Thanks & regards,
Subash P.

317 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi @subash_p ,

Could you share us the details so I can try on EVK?

Using TinyPlay, I can able to record and play WAV files from the Android 15 console.

Can you share the commands?

However, in the UI, I cannot use the microphone and speaker simultaneously.

Which UI are you using?

If I set the device speaker to SGTL5000, the recorder app cannot record (mic_in not detected). But if I disable the device speaker, I can able to record sound using the recorder app.

How do you set/disable the device speaker? What is the recorder app?

Thanks

Wish you have a nice day

Best Regards

Rita

0 项奖励
回复

418 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

I will confirm it for you