LDO-bypass mode vs LDO-enable mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LDO-bypass mode vs LDO-enable mode

6,669 Views
gregoryhermant
Contributor I

Hi All,

I was wondering how to choose between these 2 modes in a design using the PF0100 PMIC.

Indeed i don't see what are the benefits to run in LDO-bypass except to reduce power dissipation inside the iMX6.

On the other hand i read in the AN4724 : Longer power-on-hours can be achieved using LDO-enabled mode

Please help me to understand.

Greg

Labels (1)
0 Kudos
Reply
1 Reply

4,568 Views
igorpadykov
NXP Employee
NXP Employee

HI gregory

for description please look at sect.4.1.2 Linux kernel image and device tree

attached Linux Guide from L3.14.28_1.0.0_iMX6QDLS_BUNDLE

Purpose of ldo bypas is to reduce overal power consumption and heating

of processor, this is very important in portable applications.

In ldo bypas one needs to control PMIC for using Dynamic Bus Frequency and

CPU Frequency Scaling (CPUFREQ) Driver. This is described in Linux

Manual Chapter 24,25.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply