LCD interface and GPU of i.MX6Solox

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LCD interface and GPU of i.MX6Solox

1,249 Views
Musadjan
Contributor III

Hi NXP and Community friends, 

I need to understand differences between i.MX6Solox SoCs part no.  MCIMX6X1CVO08AC  and MCIMX6X3CVO08AC in terms of LCD interface. After reading information about LCD interface of the SoC in page 3 on the datasheet of the i.MX6solox , I came to conclusion that I must use SoC configuration  MCIMX6X3CVO08AC  in order to be able to implement a 7 in 24-bit display using LCD parallel interface on that SoC. The evidence for my decision is that the part MCIMX6X1CVO08AC   does not support 2D/3D GPU according to the datasheet. I would be happy if you could help me to confirm that I made right decision. or in the other world , may the part MCIMX6X1CVO08AC includes a LCD interface which can be used with that display for simple graphical tasks, like showing texts and labels.  Looking for your feedback and thanks. 

Labels (1)
0 Kudos
Reply
1 Reply

1,203 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Musadjan,

See below,please!

1. IMX6SXIEC.pdf

pastedImage_6.png

2. About LCD interface

Below is from evk schematic

pastedImage_7.png

3. eLCDIF controller inside of CPU

GPU and eLCDIF controller are different IP, eLCDIF is used to display images on lcd screen, BUT GPU is used to accelerate 2D/3D graphics.  If you just want to display simple image , not need 2D/3D acceleration.  It is no problem to choose MCIMX6X1CVO08AC.

Hope the information is helpful to you.

Have a nice day!

B.R,

Weidong