LAN9500A Linux USB Ethernet Driver Problem!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LAN9500A Linux USB Ethernet Driver Problem!

5,364件の閲覧回数
bachehkaraji
Contributor I

I'm working on a custom board equipped with a iMX28 module and the LAN9500A USB to Ethernet controller without EEPROM for the network interface. Operating system is Linux (kernel v3.16). The LAN9500A is connected to a RJ45 jack with integrated Magnetics and LEDs.

I check the reference schematics of Microchip against my design.http://ww1.microchip.com/downloads/en/DeviceDoc/9500a_sch.pdf

I can see the LAN9500A is detected and correct driver is loaded...,

# dmesg | grep -i smsc

[    1.549126] usbcore: registered new interface driver smsc95xx

[    2.186356] smsc95xx v1.0.4

[    2.258622] smsc95xx 1-1:1.0 eth2: register 'smsc95xx' at usb-ci_hdrc.1-1, smsc95xx USB 2.0 Ethernet, 62:94:6a:f1:ec:26

[    9.588663] fec 800f0000.ethernet eth0: Freescale FEC PHY driver [SMSC LAN8710/LAN8720] (mii_bus:phy_addr=800f0000.etherne:00, irq=-1)

After the system is turned on, the link and activity LEDs are lit ...

# ifconfig eth2 up

IPv6: ADDRCONF(NETDEV_UP): eth2: link is not ready

root@imx28evk:~# IPv6: ADDRCONF(NETDEV_CHANGE): eth2: link becomes ready

smsc95xx 1-1:1.0 eth2: link up, 100Mbps, full-duplex, lpa 0x4DE1

IPv6: eth2: IPv6 duplicate address fe80::fa:25ff:fe59:cf38 detected!

 

# ifconfig eth2 down

LEDs are still on ...

# ifconfig eth2 up

smsc95xx 1-1:1.0 eth2: link up, 100Mbps, full-duplex, lpa 0xC5E1

 

# ifconfig eth2 down

LEDs are still on ...

$ ifconfig eth2 up

Now the LEDs are off ...

# ethtool eth2

Settings for eth2:

        Supported ports: [ TP MII ]

        Supported link modes:   10baseT/Half 10baseT/Full

                                100baseT/Half 100baseT/Full

        Supported pause frame use: No

        Supports auto-negotiation: Yes

        Advertised link modes:  10baseT/Half 10baseT/Full

                                100baseT/Half 100baseT/Full

        Advertised pause frame use: Symmetric Receive-only

        Advertised auto-negotiation: Yes

        Speed: 10Mb/s

        Duplex: Half

        Port: MII

        PHYAD: 1

        Transceiver: internal

        Auto-negotiation: on

        Supports Wake-on: pumbag

        Wake-on: d

        Current message level: 0x00000007 (7)

                               drv probe link

        Link detected: no

 

# mii-tool eth2

eth2: no link

 

# ifconfig eth2 down

 

$ ifconfig eth2 up

smsc95xx 1-1:1.0 eth2: link up, 100Mbps, full-duplex, lpa 0xC5E1

LEDs light up

ethtool eth2

Settings for eth2:

        Supported ports: [ TP MII ]

        Supported link modes:   10baseT/Half 10baseT/Full

                                100baseT/Half 100baseT/Full

        Supported pause frame use: No

        Supports auto-negotiation: Yes

        Advertised link modes:  10baseT/Half 10baseT/Full

                                100baseT/Half 100baseT/Full

        Advertised pause frame use: Symmetric Receive-only

        Advertised auto-negotiation: Yes

        Link partner advertised link modes:  10baseT/Half 10baseT/Full

                                             100baseT/Half 100baseT/Full

        Link partner advertised pause frame use: Symmetric

        Link partner advertised auto-negotiation: Yes

        Speed: 100Mb/s

        Duplex: Full

        Port: MII

        PHYAD: 1

        Transceiver: internal

        Auto-negotiation: on

        Supports Wake-on: pumbag

        Wake-on: d

        Current message level: 0x00000007 (7)

                               drv probe link

        Link detected: yes

 

# mii-tool eth2

eth2: negotiated 1000baseT-HD flow-control, link ok

Another issue is that when I unplug and plug the Ethernet cable from the RJ45 socket, Linux does not detect it, ...

Has anyone else seen this? I really appreciate any help you can provide.

ラベル(2)
0 件の賞賛
返信
1 返信

4,328件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi bachen

kernel v3.16 is not supported by nxp, one can try on more new kernels like L4.1.15 and also

post on meta-fsl-arm mailing list, so that someone familiar with it could try to assist you.
https://lists.yoctoproject.org/listinfo/meta-freescale

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信