LAN9500A Linux USB Ethernet Driver Problem!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LAN9500A Linux USB Ethernet Driver Problem!

5,382 Views
bachehkaraji
Contributor I

I'm working on a custom board equipped with a iMX28 module and the LAN9500A USB to Ethernet controller without EEPROM for the network interface. Operating system is Linux (kernel v3.16). The LAN9500A is connected to a RJ45 jack with integrated Magnetics and LEDs.

I check the reference schematics of Microchip against my design.http://ww1.microchip.com/downloads/en/DeviceDoc/9500a_sch.pdf

I can see the LAN9500A is detected and correct driver is loaded...,

# dmesg | grep -i smsc

[    1.549126] usbcore: registered new interface driver smsc95xx

[    2.186356] smsc95xx v1.0.4

[    2.258622] smsc95xx 1-1:1.0 eth2: register 'smsc95xx' at usb-ci_hdrc.1-1, smsc95xx USB 2.0 Ethernet, 62:94:6a:f1:ec:26

[    9.588663] fec 800f0000.ethernet eth0: Freescale FEC PHY driver [SMSC LAN8710/LAN8720] (mii_bus:phy_addr=800f0000.etherne:00, irq=-1)

After the system is turned on, the link and activity LEDs are lit ...

# ifconfig eth2 up

IPv6: ADDRCONF(NETDEV_UP): eth2: link is not ready

root@imx28evk:~# IPv6: ADDRCONF(NETDEV_CHANGE): eth2: link becomes ready

smsc95xx 1-1:1.0 eth2: link up, 100Mbps, full-duplex, lpa 0x4DE1

IPv6: eth2: IPv6 duplicate address fe80::fa:25ff:fe59:cf38 detected!

 

# ifconfig eth2 down

LEDs are still on ...

# ifconfig eth2 up

smsc95xx 1-1:1.0 eth2: link up, 100Mbps, full-duplex, lpa 0xC5E1

 

# ifconfig eth2 down

LEDs are still on ...

$ ifconfig eth2 up

Now the LEDs are off ...

# ethtool eth2

Settings for eth2:

        Supported ports: [ TP MII ]

        Supported link modes:   10baseT/Half 10baseT/Full

                                100baseT/Half 100baseT/Full

        Supported pause frame use: No

        Supports auto-negotiation: Yes

        Advertised link modes:  10baseT/Half 10baseT/Full

                                100baseT/Half 100baseT/Full

        Advertised pause frame use: Symmetric Receive-only

        Advertised auto-negotiation: Yes

        Speed: 10Mb/s

        Duplex: Half

        Port: MII

        PHYAD: 1

        Transceiver: internal

        Auto-negotiation: on

        Supports Wake-on: pumbag

        Wake-on: d

        Current message level: 0x00000007 (7)

                               drv probe link

        Link detected: no

 

# mii-tool eth2

eth2: no link

 

# ifconfig eth2 down

 

$ ifconfig eth2 up

smsc95xx 1-1:1.0 eth2: link up, 100Mbps, full-duplex, lpa 0xC5E1

LEDs light up

ethtool eth2

Settings for eth2:

        Supported ports: [ TP MII ]

        Supported link modes:   10baseT/Half 10baseT/Full

                                100baseT/Half 100baseT/Full

        Supported pause frame use: No

        Supports auto-negotiation: Yes

        Advertised link modes:  10baseT/Half 10baseT/Full

                                100baseT/Half 100baseT/Full

        Advertised pause frame use: Symmetric Receive-only

        Advertised auto-negotiation: Yes

        Link partner advertised link modes:  10baseT/Half 10baseT/Full

                                             100baseT/Half 100baseT/Full

        Link partner advertised pause frame use: Symmetric

        Link partner advertised auto-negotiation: Yes

        Speed: 100Mb/s

        Duplex: Full

        Port: MII

        PHYAD: 1

        Transceiver: internal

        Auto-negotiation: on

        Supports Wake-on: pumbag

        Wake-on: d

        Current message level: 0x00000007 (7)

                               drv probe link

        Link detected: yes

 

# mii-tool eth2

eth2: negotiated 1000baseT-HD flow-control, link ok

Another issue is that when I unplug and plug the Ethernet cable from the RJ45 socket, Linux does not detect it, ...

Has anyone else seen this? I really appreciate any help you can provide.

Labels (2)
0 Kudos
Reply
1 Reply

4,346 Views
igorpadykov
NXP Employee
NXP Employee

Hi bachen

kernel v3.16 is not supported by nxp, one can try on more new kernels like L4.1.15 and also

post on meta-fsl-arm mailing list, so that someone familiar with it could try to assist you.
https://lists.yoctoproject.org/listinfo/meta-freescale

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply