LAN95 (smsc95xx) causing data corruption

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LAN95 (smsc95xx) causing data corruption

1,952件の閲覧回数
ciaran_lequeux
Contributor I

Hi,

I have a custom board with imx6 dual lite, i'm on linux.

I have a problem with data corruption in ftp download.

For my tests, in bash, i download, check md5sum and loop...

With direct network connection, i download from ftp à big file (1GB), 100% OK of all time

Now with usb ethernet adapter (LAN95), (i dissabled turbo mode, otherwise it crash)

With a 1GB file FTP : KO 100% of time
With a 60Mb file  FTP : KO 1 / 10 of time
With 1GB file with SCP : KO 1 / 5 of time

Did you have any idea why isn't working properly ?

0 件の賞賛
返信
2 返答(返信)

1,883件の閲覧回数
ciaran_lequeux
Contributor I

Hi,

 

Thanks you, but on his thread he says it's ok LAN to LAN, his command not work wih me and i'm LAN to LAN.

It's a ctusom board and i can't connect other adapters

 

I've already test with this parameters from uboot : [U-Boot] [PATCH] smsc95xx: Fetch whole burst with 1 URB, avoid framing errors (kernel.org)

Without success

 

0 件の賞賛
返信

1,920件の閲覧回数
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

Do the connections advise the same capabilities?

Could you try this setting?

I could also watch this instability here,

Have you worked with other adapters?

Regards

0 件の賞賛
返信