LAN7500 and imx6, how to implement

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LAN7500 and imx6, how to implement

3,000件の閲覧回数
alexlevandovski
Contributor I

Hello, I have imx6 Board.

on the Board i have LAN7500 chip. LAN7500 connected to imx6 USB2. Over menuconfig I included driver for LAN7500. After boot I connected Ethernet cable to LAN7500 and can see, that Ethernet Link is OK(LEDs lihtning). But if I try ping some address in Internet - Linux say me "bad address". I suppose, that I have to make some more steps to implement LAN7500.

Which steps have to be done(LAN 7500 driver is already included in .config) for full funktionality LAN7500 with imx6.

Thanks in advance.

Alex

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,584件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Alex

had you set correct mac address ?

Changing Your MAC Address/Linux - Wikibooks, open books for an open world

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,584件の閲覧回数
alexlevandovski
Contributor I

Hello Igor,  and thanks for Answer. No, I did'nt nothing - only included a driver to Linux image. How can I set mac address in boot procedure, that my Board after boot get ready to go in Internet without extra configuration from user?

best regards

alex

0 件の賞賛
返信

2,584件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Alex

please refer to p.7,9 LAN7500 datasheet

http://ww1.microchip.com/downloads/en/DeviceDoc/7500.pdf

Best regards

igor

0 件の賞賛
返信

2,584件の閲覧回数
alexlevandovski
Contributor I

Thanks for this Datasheet advice, but as I wrote both LEDs are on(Link 1GB).Somewhat another are don't made. But what?

best regards

alex

0 件の賞賛
返信