Hypervisor support in Linux BSP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hypervisor support in Linux BSP

2,591 Views
danielchempolay
Contributor II

Hi every one,

Does NXP provide any hypervisor solution for Linux BSP, can it be appended using Yocto builld system?If so, can some one provide steps to be followed to integrate hypervisor module?

Thanks in advance :smileyhappy:

Best regards,

Daniel

Labels (2)
0 Kudos
Reply
2 Replies

2,436 Views
Yuri
NXP Employee
NXP Employee

Hello,


  Hypervisor support is not provided for i.MX devices.

Please apply to  QorIQ Processing Platforms

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,436 Views
danielchempolay
Contributor II

Okay Thanks Yuri.

Regards,

Daniel

0 Kudos
Reply